4.1. tenAsys INtime
Real-time Ethernet Driver are available for INtime.
If using INtime with Windows running in parallel on the same host the network adapter card has to be assigned to INtime
The network adapters should be passed to INtime using the INtime Device Manager. Please refer to the INtime user manual for this.
Search locations for Real-time Ethernet Driver can be adjusted using the PATH environment variable
4.1.1. OS Compiler settings
Besides the general settings from OS Compiler settings the following settings are necessary to build the example application for INtime.
- Extra include paths
<InstallPath>\SDK\INC\INtime <InstallPath>\Examples\Common\INtime
- Extra source paths
<InstallPath>\Examples\Common\INtime <InstallPath>\Sources\OsLayer\INtime
- Extra library paths to the main EtherCAT components
<InstallPath>\SDK\LIB\INtime