4.7. Xenomai
The system must be setup first the same way as for EC-Simulator for Linux, especially installation of the atemsys module and Real-time Ethernet Driver usage preparation.
See also
Chapter Linux
The binaries are built using the following versions:
- armv6-vfp-eabihf:
Xenomai 2.6.3, tested on Linux Kernel 3.8.13-xenomai-2.6.4
- x64:
Xenomai 3.0.2, tested on Linux Kernel 3.18.20 (Cobalt)
EVL r0.44 (Xenomai 4), tested on Linux Kernel 5.15.106
- x86:
Xenomai 2.6.2.1, tested on Linux Kernel 3.5.7
Xenomai 3.0.2, tested on Linux Kernel 3.18.20 (Cobalt) and 3.10.32-rt31 (Mercury)
4.7.1. OS compiler settings
Besides the general settings from OS Compiler settings the following settings are necessary to build the example application for Xenomai.
- Extra include paths
<InstallPath>/SDK/INC/Xenomai <InstallPath>/Examples/Common/Xenomai
- Extra source paths
<InstallPath>/Examples/Common/Xenomai <InstallPath>/Sources/OsLayer/Xenomai
- Extra library paths to the main EtherCAT components
Xenomai 2 and 3:
<InstallPath>/SDK/LIB/Xenomai
Xenomai 4:
<InstallPath>/SDK/LIB/Xenomai4
- Extra libraries (in this order)
Xenomai 2:
EcSimulatorRasServer EcSimulator pthread dl rt native xenomai
Xenomai 3:
EcSimulatorRasServer EcSimulator pthread dl rt
xeno-config --cflagsandxeno-config --ldflagsof the Xenomai installation return the neededCFLAGSandLDFLAGS. If further information is needed, please refer to http://xenomai.org/ .Xenomai 4:
EcSimulatorRasServer EcSimulator pthread evl dl