1. Introduction
1.1. What is EtherCAT?
EtherCAT® (Ethernet for Control Automation Technology) is a high-performance Ethernet Fieldbus technology that provides a reliable, efficient, and cost-effective communication solution for a wide variety of industrial automation applications. Originally developed as an open technology by Beckhoff Automation in 2003, and subsequently turned over to an independent organization known as the EtherCAT Technology Group, EtherCAT has since become one of the most widely used industrial Ethernet protocols in the world.
See also
A comprehensive introduction to EtherCAT technology can be found at https://www.acontis.com/en/what-is-ethercat-communication-protocol.html.
1.2. EC-Simulator - Features
Feature ID: Unique identification used in ETG.1500 EtherCAT Master Classes
Feature name |
Short description |
Implemented |
Feature ID |
|---|---|---|---|
Service |
Support of all commands |
x |
101 |
IRQ field in datagram |
Use IRQ information from Slave in datagram header |
x |
102 |
Slaves with Device Emulation |
Support Slaves with and without application controller |
x |
103 |
EtherCAT State Machine |
Support of ESM special behavior |
x |
104 |
Error Handling |
Checking of network or slave errors, e.g., Working Counter |
– |
105 |
VLAN |
Support VLAN Tagging |
– |
106 |
EtherCAT Frame Types |
Support EtherCAT Frames |
x |
107 |
UDP Frame Types |
Support UDP Frames |
– |
108 |
Cyclic PDO |
Cyclic process data exchange |
x |
201 |
Multiple Tasks |
Different cycle tasks, Multiple update rates for PDO |
x |
202 |
Frame repetition |
Send cyclic frames multiple times to increase immunity |
x |
203 |
Online scanning |
Network configuration functionality included in EtherCAT Master |
x |
301 |
Reading ENI |
Network Configuration taken from ENI file |
x |
– |
Compare Network configuration |
Compare configured and existing network configuration during boot-up |
x |
302 |
Explicit Device identification |
Identification used for Hot Connect and prevention against cable swapping |
x |
303 |
Station Alias Addressing |
Support configured station alias in slave, i.e., enable 2nd Address and use it |
x |
304 |
Access to EEPROM |
Support routines to access EEPROM via ESC register |
x |
305 |
Support Mailbox |
Main functionality for mailbox transfer |
x |
401 |
Mailbox Resilient Layer |
Support underlying resilient layer |
x |
402 |
Multiple Mailbox channels |
Support multiple channels |
x |
403 |
Mailbox polling |
Polling Mailbox state in slaves |
x |
404 |
SDO Up/Download |
Normal and expedited transfer |
x |
501 |
Segmented Transfer |
Segmented transfer |
x |
502 |
Complete Access |
Transfer the entire object (with all sub-indices) at once |
x |
503 |
SDO Info service |
Services to read object dictionary |
x |
504 |
Emergency Message |
Receive Emergency messages |
x |
505 |
PDO in CoE |
PDO services transmitted via CoE |
– |
506 |
EoE protocol |
Services for tunneling Ethernet frames. Includes all specified EoE services |
x |
601 |
Virtual Switch |
Virtual Switch functionality |
– |
602 |
EoE Endpoint to Operation Systems |
Interface to the Operation System on top of the EoE layer |
– |
603 |
FoE Protocol |
Support FoE Protocol |
x |
701 |
Firmware Up-/Download |
Password, FileName should be given by the application |
x |
702 |
Boot State |
Support Boot-State for Firmware Up/Download |
x |
703 |
SoE Services |
Support SoE Services |
x |
801 |
AoE Protocol |
Support AoE Protocol |
x |
901 |
VoE Protocol |
External Connectivity supported |
x |
1001 |
DC support |
Support of Distributed Clock |
– |
1101 |
Continuous Propagation Delay |
Continuous Calculation of the compensation propagation delay |
– |
1102 |
Sync window monitoring |
Continuous monitoring of the Synchronization difference in the slaves |
– |
1103 |
via Master |
Information is given in ENI file or can be part of any other network configuration. Copying of the data can be handled by master stack or master’s application |
x |
1201 |
1.3. Editions (HiL / SiL)
1.3.1. Hardware-in-Loop (HiL) Simulation
The System-Under-Test (SUT) is communicating via an EtherCAT cable with the EC-Simulator software running on an external hardware, the HiL System. In this setup the unchanged application together with the EtherCAT master can be tested using the standard physical network interface.
1.3.2. Software-in-the-Loop (SiL) Simulation
The EtherCAT network is simulated by a software running on the System Under Test (SUT). Instead of communicating with the Ethernet Controller, the EC-Master EtherCAT master is directly exchanging EtherCAT frames with the simulation software.
1.4. Protected version
The EC-Simulator software is available in different protected versions:
- Dongled
Binary with dongle protection (Linux x64, x86, Windows only)
- Protected
Binary with MAC protection. Requires a physical network adapter for license check (HiL/SiL).
- Unrestricted:
Binary without MAC protection
The protected version is limited to 5 slaves and will automatically stop after about 10 minutes of continuous operation. In order to remove this restriction a valid runtime license key or a dongle is required. The runtime license protection with license key is based on the MAC address of the Ethernet controller used for the EtherCAT protocol. With a valid license key and Protected version the purchased features are automatically unlocked. The Dongled version needs the Dongle and WIBU service to be installed and running. The purchased features stored on the Dongle are automatically unlocked.
1.4.1. Licensing procedure for Development Licenses
Installation of EC-Simulator Protected or Dongled version accordingly
In case of EC-Simulator Protected: Determine the MAC Address by calling esGetSrcMacAddress(0, &oSrcMacAddress)/ecatGetSrcMacAddress(&oSrcMacAddress) or from a sticker applied on the hardware near the Ethernet controller.
Send an Email with the subject “Development License Key Request, Commission your commission number” with the MAC address to sales@acontis.com
Acontis will create the license keys and return them in a License Key Text File (CSV format).
Number;MAC Address;License Key 1;00-00-5A-11-77-FE;DA1099F2-15C249E9-54327FBC-3BA579B2-318AB2B6-CD13B221 2;64-31-50-80-20-4E;A2B4C98D-00185EF9-22134567-DA1099F2-15C249E9-54327FBC
Activate the License Key by calling
esSetLicenseKey()or EC_T_LINK_PARMS_SIMULATOR (SiL) with the license key that corresponds to the MAC address on the hardware and check the return code. The license key is 53 characters long. For HiL the APIesSetLicenseKey()must be called afteresInitSimulator()and beforeesConfigureNetwork(). For SiL the license key must be set atEC_T_SIMULATOR_INIT_PARMS::szLicenseKey.Example HiL:
esSetLicenseKey(0, "A2B4C98D-00185EF9-22134567-DA1099F2-15C249E9-54327FBC");
Example SiL:
$ EcMasterDemo -simulator 1 1 eni.xml --lic A2B4C98D-00185EF9-22134567-DA1099F2-15C249E9-54327FBC --link -intelgbe 1 1
1.4.2. Licensing procedure for Runtime Licenses
Installation of EC-Simulator Protected or Dongled version accordingly
In case of EC-Simulator Protected: Determine the MAC Address by calling esGetSrcMacAddress(0, &oSrcMacAddress)/ecatGetSrcMacAddress(&oSrcMacAddress) or from a sticker applied on the hardware near the Ethernet controller.
Provide the MAC Addresses and numbers from previously ordered and unused runtime license stickers in a text file to acontis as described in the example below. Please use a separate line for each runtime license sticker number and MAC Address.
100-105-1-1/1603310001;00-00-5A-11-77-FE 100-105-1-1/1603310002;64-31-50-80-20-4E
Send an Email with the subject “Runtime License Key Request, Commission your commission number” with the MAC address to sales@acontis.com
Acontis will create the license keys and return them in a License Key Text File (CSV format).
Number;MAC Address;License Key 1;00-00-5A-11-77-FE;DA1099F2-15C249E9-54327FBC 2;64-31-50-80-20-4E;A2B4C98D-00185EF9-22134567-DA1099F2-15C249E9-54327FBC
Activate the License Key by calling
esSetLicenseKey()or EC_T_LINK_PARMS_SIMULATOR (SiL) with the license key that corresponds to the MAC address on the hardware and check the return code. The license key is 53 characters long. For HiL the APIesSetLicenseKey()must be called afteresInitSimulator()and beforeesConfigureNetwork(). For SiL the license key must be set atEC_T_SIMULATOR_INIT_PARMS::szLicenseKey.Example HiL:
esSetLicenseKey(0, "A2B4C98D-00185EF9-22134567-DA1099F2-15C249E9-54327FBC");
Example SiL:
$ EcMasterDemo -simulator 1 1 eni.xml --lic A2B4C98D-00185EF9-22134567-DA1099F2-15C249E9-54327FBC --link -intelgbe 1 1
1.5. Known restrictions
Some slaves require extended information to be simulated.
The “<ExtendedInfo>”-Tag in EXI are currently not importable to EC-Engineer and must be removed before importing EXI as ENI file. Simulator settings contained in the extended information are stored in the .ecc file and can be copied between EC-Engineer instances using Copy and Paste.
Value Information (Default, Min, Max) from object dictionary cannot be retrieved using SSC, see SSC\sdoserv : “the transmission of the value info is not supported yet of the sample code”.
Occasional start up error (timeout) in case of DCM Bus Shift (DC control loop not included in EC-Simulator), work-around with OsQueryMsecCount() replacement possible.
1.6. License
1.6.1. EC-Simulator license
According to EC-Simulator Software License Agreement (SLA).
1.6.2. Free Open Source Software contained in EC-Simulator
1.6.2.1. Expat XML parser license V2.6.0
Copyright (c) 1997-2000 Thai Open Source Software Center Ltd
Copyright (c) 2000 Clark Cooper <coopercc@users.sourceforge.net>
Copyright (c) 2000-2005 Fred L. Drake, Jr. <fdrake@users.sourceforge.net>
Copyright (c) 2001-2002 Greg Stein <gstein@users.sourceforge.net>
Copyright (c) 2002-2016 Karl Waclawek <karl@waclawek.net>
Copyright (c) 2016-2024 Sebastian Pipping <sebastian@pipping.org>
Copyright (c) 2016 Cristian Rodríguez <crrodriguez@opensuse.org>
Copyright (c) 2016 Thomas Beutlich <tc@tbeu.de>
Copyright (c) 2017 Rhodri James <rhodri@wildebeest.org.uk>
Copyright (c) 2022 Thijs Schreijer <thijs@thijsschreijer.nl>
Copyright (c) 2023 Hanno Böck <hanno@gentoo.org>
Copyright (c) 2023 Sony Corporation / Snild Dolkow <snild@sony.com>
Licensed under the MIT license:
Permission is hereby granted, free of charge, to any person obtaining
a copy of this software and associated documentation files (the
"Software"), to deal in the Software without restriction, including
without limitation the rights to use, copy, modify, merge, publish,
distribute, sublicense, and/or sell copies of the Software, and to permit
persons to whom the Software is furnished to do so, subject to the
following conditions:
The above copyright notice and this permission notice shall be included
in all copies or substantial portions of the Software.
THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND,
EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF
MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN
NO EVENT SHALL THE AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM,
DAMAGES OR OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR
OTHERWISE, ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE
USE OR OTHER DEALINGS IN THE SOFTWARE.
1.6.3. Free Open Source Software supported by EC-Simulator
The following components are not part of EC-Simulator, but relate to it:
1.6.3.1. acontis atemsys Linux kernel module
The acontis atemsys is licensed under the GPL:
Copyright (c) 2009 - 2020 acontis technologies GmbH, Ravensburg, Germany
All rights reserved.
This program is free software; you can redistribute it and/or modify it
under the terms of the GNU General Public License as published by the
Free Software Foundation; either version 2 of the License, or (at your
option) any later version.
1.6.3.2. WinPCap
The WinPCap library is supported, but not shipped with EC-Simulator.
1.6.3.3. Npcap
The Npcap library is supported, but not shipped with EC-Simulator.
1.7. Versioning
EC-Simulator follows the following versioning scheme: VMAJOR. MINOR. SERVICEPACK. BUILD (e.g. V3.2.1.04).
The libraries are binary compatible by unchanged MAJOR and MINOR digits. If SERVICEPACK increments, BUILD restarts with 01. BUILD 99 is reserved for test builds that have not been officially released for productive usage.