6.9. Slave control and status functions
6.9.1. esGetNumConfiguredSlaves
6.9.2. esGetNumConnectedSlaves
6.9.3. esGetSlaveId
-
EC_T_DWORD esGetSlaveId(EC_T_DWORD dwInstanceID, EC_T_WORD wStationAddress)
Determines the slave ID using the slave station address.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
wStationAddress – [in] Station address of the slave
- Returns:
Slave ID or INVALID_SLAVE_ID if the slave could not be found or stack is not initialized
Example
/* get slave id of slave with station address 1001 */
EC_T_DWORD dwSlaveId = esGetSlaveId(dwSimulatorId, 1001);
if (INVALID_SLAVE_ID == dwSlaveId)
{
dwRetVal = EC_E_NOTFOUND;
goto Exit;
}
6.9.4. esGetSlaveIdAtPosition
-
EC_T_DWORD esGetSlaveIdAtPosition(EC_T_DWORD dwInstanceID, EC_T_WORD wAutoIncAddress)
Determines the slave ID using the slave auto increment address.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
wAutoIncAddress – [in] Auto increment address of the slave
- Returns:
Slave ID or INVALID_SLAVE_ID if no slave matching wAutoIncAddress can be found
Example
/* get slave id of third slave (auto inc address 0, -1, -2, ...) */
EC_T_DWORD dwSlaveId = esGetSlaveIdAtPosition(dwSimulatorId, (EC_T_WORD)-2);
if (INVALID_SLAVE_ID == dwSlaveId)
{
dwRetVal = EC_E_NOTFOUND;
goto Exit;
}
6.9.5. esGetSlaveState
-
EC_T_DWORD esGetSlaveState(EC_T_DWORD dwInstanceID, EC_T_DWORD dwSlaveId, EC_T_WORD *pwCurrDevState, EC_T_WORD *pwReqDevState)
Get the slave state.
The slave state is always read automatically from the AL_STATUS register whenever necessary. It is not forced by calling this function. This function may be called from within the JobTask’s context.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwSlaveId – [in] Slave ID
pwCurrDevState – [out] Current slave state.
pwReqDevState – [out] Requested slave state
- Returns:
EC_E_NOERROR if successful.
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the output pointers are EC_NULL
EC_E_SLAVE_NOT_PRESENT if slave not present.
EC_E_NOTFOUND if no slave matching dwSlaveId can be found
6.9.6. esSetSlaveState
-
EC_T_DWORD esSetSlaveState(EC_T_DWORD dwInstanceID, EC_T_DWORD dwSlaveId, EC_T_WORD wDeviceState, EC_T_DWORD dwTimeout)
Set a specified slave into the requested EtherCAT state.
The requested state shall not be higher than the overall operational state. DEVICE_STATE_BOOTSTRAP can only be requested if the slave’s state is INIT. This function may not be called from within the JobTask’s context.
If the function is called with EC_NOWAIT, the client may wait for reaching the requested state using the notification callback (EC_NOTIFY_SLAVE_STATECHANGED).
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwSlaveId – [in] Slave ID
wDeviceState – [in] Requested device state. See DEVICE_STATE_…
dwTimeout – [in] Timeout [ms] This function will block until the requested state is reached or the timeout elapsed. If the timeout value is set to EC_NOWAIT the function will return immediately.
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized or denies the requested state, see comments below
EC_E_INVALIDPARM if dwInstanceID is out of range or BOOTSTRAP was requested for a slave that does not support it
EC_E_NOTFOUND if no slave matching dwSlaveId can be found
EC_E_TIMEOUT if dwTimeout elapsed during the API call
EC_E_BUSY if the EtherCAT stack cannot execute the request at this time, the function has to be called at a later time
EC_E_NOTREADY if the working counter was not set when requesting the slave’s state (slave may not be connected or did not respond)
EC_E_MASTER_RED_STATE_INACTIVE if Master Redundancy is configured and master is inactive
6.9.7. esIsSlavePresent
-
EC_T_DWORD esIsSlavePresent(EC_T_DWORD dwInstanceID, EC_T_DWORD dwSlaveId, EC_T_BOOL *pbPresence)
Returns whether a specific slave is currently connected to the Bus.
This function may be called from within the JobTask.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwSlaveId – [in] Slave ID
pbPresence – [out] EC_TRUE if slave is currently connected to the bus, EC_FALSE if not.
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range
EC_E_NOTFOUND if no slave matching dwSlaveId can be found
6.9.8. esGetSlaveProp
-
EC_T_BOOL esGetSlaveProp(EC_T_DWORD dwInstanceID, EC_T_DWORD dwSlaveId, EC_T_SLAVE_PROP *pSlaveProp)
Determines the properties of the slave device.
deprecated Use esGetCfgSlaveInfo instead
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwSlaveId – [in] Slave ID
pSlaveProp – [out] Slave properties
- Returns:
EC_TRUE if the slave exists, EC_FALSE if no slave matching dwSlaveId can be found
6.9.9. esGetSlavePortState
-
EC_T_DWORD esGetSlavePortState(EC_T_DWORD dwInstanceID, EC_T_DWORD dwSlaveId, EC_T_WORD *pwPortState)
Returns the state of the slave ports.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwSlaveId – [in] Slave ID
pwPortState –
[out] Slave port state.
Format: wwww xxxx yyyy zzzz (each nibble : port 3210)
wwww : Signal detected 1=yes, 0=no (ESC Register 0x110 Bit 9, 11, 13, 15)
xxxx : Loop closed 1=yes, 0=no (ESC Register 0x110 Bit 8, 10, 12, 14)
yyyy : Link established 1=yes, 0=no (ESC Register 0x110 Bit 4, 5, 6, 7)
zzzz : Slave connected 1=yes, 0=no (zzzz = logical result of w,x,y)
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the output pointer is EC_NULL
EC_E_NOTFOUND if no slave matching dwSlaveId can be found
6.9.10. esGetSlaveInpVarInfoNumOf
-
EC_T_DWORD esGetSlaveInpVarInfoNumOf(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_WORD *pwSlaveInpVarInfoNumOf)
Gets the number of input variables of a specific slave.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
pwSlaveInpVarInfoNumOf – [out] Number of found process variable entries
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the output pointer is EC_NULL
EC_E_NOTFOUND if no slave matching bFixedAddressing / wSlaveAddress can be found
6.9.11. esGetSlaveOutpVarInfoNumOf
-
EC_T_DWORD esGetSlaveOutpVarInfoNumOf(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_WORD *pwSlaveOutpVarInfoNumOf)
Gets the number of output variables of a specific slave.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
pwSlaveOutpVarInfoNumOf – [out] Number of found process variables
- Returns:
EC_E_NOERROR or error code
6.9.12. esGetSlaveInpVarInfo
-
EC_T_DWORD esGetSlaveInpVarInfo(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_WORD wNumOfVarsToRead, EC_T_PROCESS_VAR_INFO *pSlaveProcVarInfoEntries, EC_T_WORD *pwReadEntries)
Gets the process variable information entries of an specific slave.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
wNumOfVarsToRead – [in] Number process variable entries that have been stored in pSlaveProcVarInfoEntries
pSlaveProcVarInfoEntries – [out] The read process variable information entries
pwReadEntries – [out] The number of read process variable information entries
- Returns:
EC_E_NOERROR or error code
6.9.13. esGetSlaveInpVarInfoEx
-
EC_T_DWORD esGetSlaveInpVarInfoEx(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_WORD wNumOfVarsToRead, EC_T_PROCESS_VAR_INFO_EX *pSlaveProcVarInfoEntriesEx, EC_T_WORD *pwReadEntries)
Gets the input process variable extended information entries of a specific slave.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
wNumOfVarsToRead – [in] Number process variable entries that have been stored in pSlaveProcVarInfoEntries
pSlaveProcVarInfoEntriesEx – [out] The read process variable extended information entries
pwReadEntries – [out] The number of read process variable information entries
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the output pointer is EC_NULL
EC_E_NOTFOUND if no slave matching bFixedAddressing / wSlaveAddress can be found
-
struct EC_T_PROCESS_VAR_INFO_EX
Public Members
-
EC_T_WORD wDataType
[out] Data type of the found process variable (according to ETG.1000, section 5). See also EcCommon.h, DEFTYPE_BOOLEAN
-
EC_T_BOOL bIsInputData
[out] Determines whether the found process variable is an input variable or an output variable
-
EC_T_WORD wDataType
6.9.14. esGetSlaveOutpVarInfo
-
EC_T_DWORD esGetSlaveOutpVarInfo(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_WORD wNumOfVarsToRead, EC_T_PROCESS_VAR_INFO *pSlaveProcVarInfoEntries, EC_T_WORD *pwReadEntries)
Gets the output process variable information entries of a specific slave.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
wNumOfVarsToRead – [in] Number of found process variable entries
pSlaveProcVarInfoEntries – [out] The read process variable information entries
pwReadEntries – [out] The number of read process variable information entries
- Returns:
EC_E_NOERROR or error code
See also
6.9.15. esGetSlaveOutpVarInfoEx
-
EC_T_DWORD esGetSlaveOutpVarInfoEx(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_WORD wNumOfVarsToRead, EC_T_PROCESS_VAR_INFO_EX *pSlaveProcVarInfoEntriesEx, EC_T_WORD *pwReadEntries)
Gets the output process variable extended information entries of a specific slave.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
wNumOfVarsToRead – [in] Number of process variable information entries
pSlaveProcVarInfoEntriesEx – [out] The read process extended variable entries
pwReadEntries – [out] The number of read process variable information entries
- Returns:
EC_E_NOERROR or error code
See also
6.9.16. esGetSlaveInpVarByObjectEx
-
EC_T_DWORD esGetSlaveInpVarByObjectEx(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_WORD wIndex, EC_T_WORD wSubIndex, EC_T_PROCESS_VAR_INFO_EX *pProcessVarInfoEntry)
Gets the input process variable extended information entry by object index, subindex of a specific slave.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
wIndex – [in] Object Index
wSubIndex – [in] Object SubIndex
pProcessVarInfoEntry – [out] Process variable extended information entry
- Returns:
EC_E_NOERROR or error code
See also
6.9.17. esGetSlaveOutpVarByObjectEx
-
EC_T_DWORD esGetSlaveOutpVarByObjectEx(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_WORD wIndex, EC_T_WORD wSubIndex, EC_T_PROCESS_VAR_INFO_EX *pProcessVarInfoEntry)
Gets the input process variable extended information entry by object index, subindex of a specific slave.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
wIndex – [in] Object Index
wSubIndex – [in] Object SubIndex
pProcessVarInfoEntry – [out] Process variable extended information entry
- Returns:
EC_E_NOERROR or error code
See also
6.9.18. esFindInpVarByName
-
EC_T_DWORD esFindInpVarByName(EC_T_DWORD dwInstanceID, const EC_T_CHAR *szVariableName, EC_T_PROCESS_VAR_INFO *pProcessVarInfoEntry)
Finds an input process variable information entry by the variable name.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
szVariableName – [in] Variable name
pProcessVarInfoEntry – [out] Process variable information entry
- Returns:
EC_E_NOERROR or error code
See also
6.9.19. esFindInpVarByNameEx
-
EC_T_DWORD esFindInpVarByNameEx(EC_T_DWORD dwInstanceID, const EC_T_CHAR *szVariableName, EC_T_PROCESS_VAR_INFO_EX *pProcessVarInfoEntry)
Finds an input process variable extended information entry by the variable name.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
szVariableName – [in] Variable name
pProcessVarInfoEntry – [out] Process variable extended information entry
- Returns:
EC_E_NOERROR or error code
See also
6.9.20. esFindOutpVarByName
-
EC_T_DWORD esFindOutpVarByName(EC_T_DWORD dwInstanceID, const EC_T_CHAR *szVariableName, EC_T_PROCESS_VAR_INFO *pProcessVarInfoEntry)
Finds an output process variable information entry by the variable name.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
szVariableName – [in] Variable name
pProcessVarInfoEntry – [out] Process variable information entry
- Returns:
EC_E_NOERROR or error code
See also
6.9.21. esFindOutpVarByNameEx
-
EC_T_DWORD esFindOutpVarByNameEx(EC_T_DWORD dwInstanceID, const EC_T_CHAR *szVariableName, EC_T_PROCESS_VAR_INFO_EX *pProcessVarInfoEntry)
Finds an output process variable extended information entry by the variable name.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
szVariableName – [in] Variable name
pProcessVarInfoEntry – [out] Process variable extended information entry
- Returns:
EC_E_NOERROR or error code
See also
6.9.22. esWriteSlaveRegister
Warning
Changing contents of ESC registers may lead to unpredictiable behavior of the slaves and/or the master.
-
EC_T_DWORD esWriteSlaveRegister(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_WORD wRegisterOffset, EC_T_BYTE *pbyData, EC_T_WORD wLen, EC_T_DWORD dwTimeout)
Writes data into the ESC memory of a specified slave.
This function may not be called from within the JobTask’s context
Warning
Changing contents of ESC registers may lead to unpredictable behavior of the slaves and/or the master.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
wRegisterOffset – [in] Register offset, e.g. use 0x0120 to write to the AL Control register.
pbyData – [in] Buffer containing transferred data
wLen – [in] Number of bytes to send
dwTimeout – [in] Timeout [ms]
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the command is not supported or the timeout value is set to EC_NOWAIT
EC_E_SLAVE_NOT_PRESENT if slave not present
EC_E_NOTFOUND if no slave matching bFixedAddressing / wSlaveAddress can be found
EC_E_TIMEOUT if dwTimeout elapsed during the API call
EC_E_BUSY another transfer request is already pending or the EtherCAT stack or the corresponding slave is currently changing its operational state
EC_E_NOTREADY if the working counter was not set when sending the command (slave may not be connected or did not respond)
EC_E_INVALIDSIZE if the size of the complete command does not fit into a single Ethernet frame. The maximum amount of data to transfer must not exceed 1486 bytes
6.9.23. esReadSlaveRegister
-
EC_T_DWORD esReadSlaveRegister(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_WORD wRegisterOffset, EC_T_BYTE *pbyData, EC_T_WORD wLen, EC_T_DWORD dwTimeout)
Reads data from the ESC memory of a specified slave.
This function may not be called from within the JobTask’s context.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
wRegisterOffset – [in] Register offset. I.e. use 0x0130 to read the AL Status register.
pbyData – [out] Buffer receiving transferred data
wLen – [in] Number of bytes to receive
dwTimeout – [in] Timeout [ms]
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the command is not supported or the timeout value is set to EC_NOWAIT
EC_E_SLAVE_NOT_PRESENT if slave not present
EC_E_NOTFOUND if no slave matching bFixedAddressing / wSlaveAddress can be found
EC_E_TIMEOUT if dwTimeout elapsed during the API call
EC_E_BUSY another transfer request is already pending or the EtherCAT stack or the corresponding slave is currently changing its operational state
EC_E_NOTREADY if the working counter was not set when sending the command (slave may not be connected or did not respond)
EC_E_INVALIDSIZE if the size of the complete command does not fit into a single Ethernet frame. The maximum amount of data to transfer must not exceed 1486 bytes
6.9.24. esReadSlaveEEPRom
-
EC_T_DWORD esReadSlaveEEPRom(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_WORD wEEPRomStartOffset, EC_T_WORD *pwReadData, EC_T_DWORD dwReadLen, EC_T_DWORD *pdwNumOutData, EC_T_DWORD dwTimeout)
Read EEPROM data from slave.
This function may not be called from within the JobTask’s context.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
wEEPRomStartOffset – [in] Word address to start EEPROM read from
pwReadData – [in] Pointer to EC_T_WORD array to carry the read data
dwReadLen – [in] Size of the EC_T_WORD array provided at pwReadData (in EC_T_WORDs)
pdwNumOutData – [out] Pointer to EC_T_DWORD carrying actually read data (in EC_T_WORDs) after completion
dwTimeout – [in] Timeout [ms]. The function will block at most for this time. The timeout value must not be set to EC_NOWAIT.
- Returns:
EC_E_NOERROR or error code
6.9.25. esWriteSlaveEEPRom
-
EC_T_DWORD esWriteSlaveEEPRom(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_WORD wEEPRomStartOffset, EC_T_WORD *pwWriteData, EC_T_DWORD dwWriteLen, EC_T_DWORD dwTimeout)
Write EEPROM data to slave.
This function may not be called from within the JobTask’s context.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
wEEPRomStartOffset – [in] Word address to start EEPROM Write from
pwWriteData – [in] Pointer to WORD array carrying the write data
dwWriteLen – [in] Size of Write Data WORD array (in WORDS)
dwTimeout – [in] Timeout [ms]. The function will block at most for this time. The timeout value must not be set to EC_NOWAIT.
- Returns:
EC_E_NOERROR or error code
Note
The EEPROM’s CRC at word 7 is re-calculated automatically if the written data is completely within the ESC Configuration Area in the EEPROM’s SII.
6.9.26. esGetSimSlaveInfo
-
EC_T_DWORD esGetSimSlaveInfo(EC_T_DWORD dwInstanceId, EC_T_WORD wCfgFixedAddress, EC_T_SIM_SLAVE_INFO *pSimSlaveInfo)
Get extended configuration and status information for slave from simulator.
- Parameters:
dwInstanceId – [in] Simulator Instance ID
wCfgFixedAddress – [in] Slave’s station address
pSimSlaveInfo – [out] Extended configuration and status information for slave from simulator
- Returns:
EC_E_NOERROR or error code
Content of EC_T_SIM_SLAVE_INFO, EC_T_SIM_SLAVE_CFG_INFO, EC_T_SIM_SLAVE_STATUS_INFO is subject to be extended.
-
struct EC_T_SIM_SLAVE_INFO
Public Members
-
EC_T_SIM_SLAVE_CFG_INFO oCfg
[out] Config Info (ENI/EXI)
-
EC_T_SIM_SLAVE_STATUS_INFO oStatus
[out] Status Info
-
EC_T_SIM_SLAVE_CFG_INFO oCfg
-
struct EC_T_SIM_SLAVE_CFG_INFO
Public Members
-
EC_T_WORD wFixedAddress
[out] Slave’s station address (ENI/EXI: /EtherCATConfig/Config/Slave/Info/PhysAddr)
-
EC_T_BOOL bPowerOff
[out] Slave powered off on startup (EXI: /EtherCATConfig/ExtendedConfig/Slaves/Slave@PowerOff)
-
EC_T_BOOL bSimulated
[out] Slave is simulated (EXI: /EtherCATConfig/ExtendedConfig/Slaves/Slave/Simulated)
-
EC_T_BOOL bIgnoreCoeDownloadError
[out] Slave ignores CoE download errors (EXI: /EtherCATConfig/ExtendedConfig/Slaves/Slave/Mailbox/CoE@IgnoreDownloadError)
-
EC_T_SIMULATOR_DEVICE_CONNECTION_DESC aPortConnection[4]
[out] Explicit port connection (optional) (EXI: /EtherCATConfig/ExtendedConfig/Slaves/Slave/PortConnection)
-
EC_T_CHAR szApplicationName[EC_SIM_SLAVE_CFG_APP_NAME_SIZE]
[out] Configured slave application name (EXI: /EtherCATConfig/ExtendedConfig/Slaves/Slave/Application/Name)
-
EC_T_WORD wFixedAddress
-
struct EC_T_SIM_SLAVE_STATUS_INFO
Public Members
-
EC_T_BOOL bIsPresent
[out] Slave is present in topology segment and connected to the network. See esConnectPorts(), Hot Connect.
-
EC_T_WORD wAlStatusReq
[out] AL Status (0x0130) requested from Simulator application. See esSetSimSlaveState()
-
EC_T_BOOL bIsPresent
6.9.27. esGetBusSlaveInfo
-
EC_T_DWORD esGetBusSlaveInfo(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_BUS_SLAVE_INFO *pSlaveInfo)
Return information about a slave connected to the EtherCAT bus.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
pSlaveInfo – [out] Information from the slave.
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range
EC_E_NOTFOUND if no slave matching bFixedAddressing / wSlaveAddress can be found
Content of EC_T_BUS_SLAVE_INFO is subject to be extended.
-
struct EC_T_BUS_SLAVE_INFO
Public Members
-
EC_T_DWORD adwPortSlaveIds[ESC_PORT_COUNT]
[out] The slave’s ID of the slaves connected to ports. See Port slave ID’s
-
EC_T_WORD wPortState
[out] Port link state. Format: wwww xxxx yyyy zzzz (each nibble : port 3210)
wwww : Signal detected 1=yes, 0=no
xxxx : Loop closed 1=yes, 0=no
yyyy : Link established 1=yes, 0=no
zzzz : Slave connected 1=yes, 0=no (zzzz = logical result of w,x,y)
-
EC_T_WORD wAlStatusCode
[out] AL status code. (Value of slave ESC register 0x0134 during last error acknowledge). This value is reset after a slave state change
-
EC_T_DWORD dwSystemTimeDifference
[out] System time difference. (Value of slave ESC register 0x092C)
-
EC_T_WORD wMbxSupportedProtocols
[out] Supported Mailbox Protocols stored in the EEPROM at offset 0x001C
-
EC_T_WORD wIdentifyData
[out] Last read identification value see EC_T_CFG_SLAVE_INFO.wIdentifyAdo
-
EC_T_DWORD dwSlaveDelay
[out] Delay behind slave [ns]. This value is only valid if a DC configuration is used
-
EC_T_DWORD dwPropagDelay
[out] Propagation delay [ns]. ESC register 0x0928,This value is only valid if a DC configuration is used
-
EC_T_DWORD adwPortSlaveIds[ESC_PORT_COUNT]
Get bus slave info with station address example
EC_T_BUS_SLAVE_INFO oBusSlaveInfo;
/* get bus slave info of slave with station address 1001 */
dwRes = esGetBusSlaveInfo(dwSimulatorId, EC_TRUE, 1001, &oBusSlaveInfo);
if (dwRes != EC_E_NOERROR)
{
dwRetVal = dwRes;
goto Exit;
}
Get bus slave info with auto-inc address example
EC_T_BUS_SLAVE_INFO oBusSlaveInfo;
/* get bus slave info of third slave (auto inc address 0, -1, -2, ...) */
dwRes = esGetBusSlaveInfo(dwSimulatorId, EC_FALSE, (EC_T_WORD)-2, &oBusSlaveInfo);
if (dwRes != EC_E_NOERROR)
{
dwRetVal = dwRes;
goto Exit;
}
6.9.28. esReadSlaveIdentification
-
EC_T_DWORD esReadSlaveIdentification(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_WORD wAdo, EC_T_WORD *pwValue, EC_T_DWORD dwTimeout)
Read identification value from slave.
This function may not be called from within the JobTask’s context.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
wAdo – [in] ADO used for identification command
pwValue – [out] Pointer to Word value containing the Identification value
dwTimeout – [in] Timeout [ms]
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range or the command is not supported or the timeout value is set to EC_NOWAIT
EC_E_SLAVE_NOT_PRESENT if slave not present
EC_E_NOTFOUND if no slave matching bFixedAddressing / wSlaveAddress can be found
EC_E_TIMEOUT if dwTimeout elapsed during the API call
EC_E_BUSY another transfer request is already pending or the EtherCAT stack or the corresponding slave is currently changing its operational state
EC_E_NOTREADY if the working counter was not set when sending the command (slave may not be connected or did not respond)
EC_E_ADO_NOT_SUPPORTED if the slave does not support requesting ID mechanism
EC_E_MASTER_RED_STATE_INACTIVE if Master Redundancy is configured and master is inactive
6.9.29. esGetSlaveStatistics
-
EC_T_DWORD esGetSlaveStatistics(EC_T_DWORD dwInstanceID, EC_T_DWORD dwSlaveId, EC_T_SLVSTATISTICS_DESC *pSlaveStatisticsDesc)
Get Slave’s statistics counter.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwSlaveId – [in] Slave id
pSlaveStatisticsDesc – [out] Pointer to structure EC_T_SLVSTATISTICS_DESC
- Returns:
EC_E_NOERROR or error code
6.9.30. esClearSlaveStatistics
-
EC_T_DWORD esClearSlaveStatistics(EC_T_DWORD dwInstanceID, EC_T_DWORD dwSlaveId)
Clears all error registers of a slave.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwSlaveId – [in] Slave Id, INVALID_SLAVE_ID clears all slaves
- Returns:
EC_E_NOERROR or error code