5.2. Broadcom Genet - emllBcmGenet
The parameters to the Real-time Ethernet Driver Broadcom® Genet are setup-specific.
The function CreateLinkParmsFromCmdLineBcmGenet() in EcSelectLinkLayer.cpp demonstrates how to initialize the Real-time Ethernet Driver instance.
-
struct EC_T_LINK_PARMS_BCMGENET
Public Members
-
EC_T_LINK_PARMS linkParms
Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_BCMGENET
-
EC_T_BCMGENET_TYPE eSocType
Broadcom processor type
-
EC_T_BOOL bNotUseDmaBuffers
EC_FALSE: Use buffers from DMA for receive (default), EC_TRUE: use buffers from heap for receive. EcLinkAllocSendFrame is not supported if bNotUseDmaBuffers = EC_TRUE.
-
EC_T_PHYINTERFACE ePhyInterface
PHY interface type
-
EC_T_LINK_PARMS linkParms