5.22. Beckhoff CUxxxx Multiplier - emllMultiplier

The parameters to the Multiplier Real-time Ethernet Driver are setup-specific. The function “CreateLinkParmsFromCmdLineMultiplier” in EcSelectLinkLayer.cpp demonstrates how to initialize the Real-time Ethernet Driver instance.

Public Members

Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_MULTIPLIER.

Type of the Multiplier Ethernet port

Used CU2508 downlink port

Link parameters of network adapter connected to the uplink of the Multiplier

enum EC_T_MULTIPLIER_TYPE

Values:

enumerator eMultiplier_Cu2508

Beckhoff CU2508 port multiplier

enumerator eMultiplier_Et2000

Beckhoff ET2000 industrial Ethernet multi-channel probe

5.22.1. Configuration with EC-Engineer

This configuration is valid for one downlink port. For each used CUxxxx multiplier downlink port, a new configuration should be arranged.

  • Start EC-Engineer in Offline Configuration modus.

  • Add the CU2508 Ethernet Port as your first SubDevice.

EC-Engineer Offline Configuration showing the CU2508 Ethernet Port SubDevice added as the first device in the network topology
  • Append the SubDevices that you are going to connect to the port.

EC-Engineer configuration showing SubDevices appended to the CU2508 downlink port for Multiplier Real-time Ethernet Driver setup