5.32. Linux SockXdp - emllSockXdp
The Real-time Ethernet Driver SockXdp does not need the atemsys driver and uses already established Ethernet adapters, e.g. eth0, eth1, etc. It is strongly recommended to use a separate network adapter to connect EtherCAT® network adapters. If the main network adapter is used for both EtherCAT® network adapters and the local area network there may be a major impact on the local area network operation.
Note
Root privileges are required.
The parameters to the Real-time Ethernet Driver SockXdp are setup-specific. The function CreateLinkParmsFromCmdLineSockXdp() in EcSelectLinkLayer.cpp demonstrates how to initialize the Real-time Ethernet Driver instance.
-
struct EC_T_LINK_PARMS_SOCKXDP
Public Members
-
EC_T_LINK_PARMS linkParms
Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_SOCKXDP.
-
EC_T_CHAR szAdapterName[EC_SOCKXDP_ADAPTER_NAME_SIZE]
Native ETH device name, e.g. “eth0” (zero terminated)
-
EC_T_WORD wQueueId
Used NIC Queue Id
-
EC_T_XDP_MODE eXdpMode
XDP mode
-
EC_T_BOOL bDisableForceBroadcast
Don’t change target MAC address to FF:FF:FF:FF:FF:FF
-
EC_T_BOOL bReplacePaddingWithNopCmd
Prevent adding Ethernet padding to work-around EtherCAT corruption bugs from native Linux driver(s)
-
EC_T_LINK_PARMS linkParms
-
enum EC_T_XDP_MODE
Values:
-
enumerator eXDP_SKB_MODE
Generic XDP, XDP runs in the standard network stack. This is the fallback mode if native XDP is not supported
-
enumerator eXDP_DRV_MODE
Native XDP, Runs XDP directly in the NIC driver. This is the recommended mode for the best performance
-
enumerator eXDP_SKB_MODE
5.32.1. Linux System Requirements
To use the XDP Real-time Ethernet Driver the following system requirements need to be met:
- Your kernel have to support XDP, check if the following entry is activated in your
.configfile. CONFIG_XDP_SOCKETS=yIf it is not activated you need to rebuild your kernel with
CONFIG_XDP_SOCKETS.
- Your kernel have to support XDP, check if the following entry is activated in your
5.32.2. Getting started
Download libxdp Version 1.4.3 from xdp-project/xdp-tools and install it.
Download libbpf Version 1.5.0 from libbpf/libbpf and install it.
Update the linux drivers of the NIC that would be used
- If the NIC supports XDP, turn off xdp generic mode:
$ ip link set dev eth0 xdpgeneric off
- If the NIC have multiple queue support, use one queue instead of multiple queues:
$ ethtool -L eth0 combined 1