4.17. Xenomai

The system must be setup first the same way as for EC-Master for Linux, especially installation of the atemsys module and Real-time Ethernet Driver usage preparation.

See also

Chapter Linux

The binaries are built using the following versions:

  • x64:
    • Xenomai 3.0.2, tested on Linux Kernel 3.18.20 (Cobalt)

    • EVL r0.44 (Xenomai 4), tested on Linux Kernel 5.15.106

  • x86:
    • Xenomai 2.6.2.1, tested on Linux Kernel 3.5.7

    • Xenomai 3.0.2, tested on Linux Kernel 3.18.20 (Cobalt) and 3.10.32-rt31 (Mercury)

4.17.1. Setting up and running EcMasterDemo

  1. Prepare system

    Prepare the system to run EcMasterDemo on Linux as described in chapter Linux

  2. Compile EcMasterDemo

    As a starting point there is the Eclipse project for EcMasterDemo for Xenomai located at Workspace/Xenomai/. Ensure OPERATING_SYSTEM, ARCH, CFLAGS, LDFLAGS, LD_LIBRARY_PATH are set accordingly (export ARCH=x86, …) when compiling using Eclipse! For Xenomai 4 the environment variable ELV_PATH should contain path of the libevl. Also ensure the following define is present:

    EC_OS_VERSION=4
    
  3. Run using GDB

    Provide search path for Xenomai libraries and prevent GDB to stop execution on SIGXCPU:

    export LD_LIBRARY_PATH=../../Bin/Xenomai/x86:/usr/xenomai/lib:.
    gdb --args ./EcMasterDemo -intelgbe 2 1 -f eni.xml -v 3
    [...]
    (gdb) handle SIGXCPU nostop noprint nopass
    (gdb) run
    

4.17.2. OS compiler settings

Besides the general settings from Compiling the EcMasterDemo the following settings are necessary to build the example application for Xenomai.

Extra include paths
<InstallPath>/SDK/INC/Xenomai
<InstallPath>/Examples/Common/Xenomai
Extra source paths
<InstallPath>/Examples/Common/Xenomai
<InstallPath>/Sources/OsLayer/Xenomai
Extra library paths to the main EtherCAT® components
  • Xenomai 2 and 3:

<InstallPath>/SDK/LIB/Xenomai
  • Xenomai 4:

<InstallPath>/SDK/LIB/Xenomai4
Extra libraries (in this order)
  • Xenomai 2:

EcMasterRasServer EcMaster pthread dl rt native xenomai
  • Xenomai 3:

EcMasterRasServer EcMaster pthread dl rt
xeno-config --cflags and xeno-config --ldflags of the Xenomai installation return the needed CFLAGS and LDFLAGS. If further information is needed, please refer to http://xenomai.org/ .
  • Xenomai 4:

EcMasterRasServer EcMaster pthread evl dl