6.16. EtherCAT® Bus Scan
The acontis EtherCAT® MainDevice stack supports scanning the EtherCAT® Bus to determine which SubDevices are available. If a configuration was provided the connected SubDevices are validated against the given ENI.
See also
6.16.1. emIoCtl - EC_IOCTL_SB_ENABLE
-
EC_IOCTL_SB_ENABLE
Enables Busscan support.
- Parameters:
pbyInBuf – [in] Pointer to Timeout Parameter Value [ms] (EC_T_DWORD). Timeout Parameter is used for timeout during Bus Topology determination.
dwInBufSize – [in] Size of the input buffer provided at pbyInBuf in bytes
pbyOutBuf – [out] Should be set to EC_NULL
dwOutBufSize – [in] Should be set to 0
pdwNumOutData – [out] Should be set to EC_NULL
- Returns:
EC_E_NOERROR or error code
The bus scan support is enabled by default.
6.16.2. emIoCtl - EC_IOCTL_SB_RESTART
-
EC_IOCTL_SB_RESTART
Start scanning the network (again). On completion the Notfication EC_NOTIFY_SB_STATUS is given.
- Parameters:
pbyInBuf – [in] Should be set to EC_NULL
dwInBufSize – [in] Should be set to 0
pbyOutBuf – [out] Should be set to EC_NULL
dwOutBufSize – [in] Should be set to 0
pdwNumOutData – [out] Should be set to EC_NULL
- Returns:
EC_E_NOERROR or error code
The timeout value given by emIoCtl - EC_IOCTL_SB_ENABLE will be used.
This function may be called prior to running emConfigureNetwork(). In such a case a first bus scan will be executed before MainDevice configuration. This feature may be used to dynamically create or adjust the XML configuration file. When issuing this IoCtl, the application has to take care emExecJob() is called cyclically to trigger MainDevice state machines, timers, send acyclic and receive frames accordingly.
6.16.3. emIoCtl - EC_IOCTL_SB_STATUS_GET
-
EC_IOCTL_SB_STATUS_GET
Get the status of the last bus scan.
- Parameters:
pbyInBuf – [in] Should be set to EC_NULL
dwInBufSize – [in] Should be set to 0
pbyOutBuf – [out] Pointer to EC_T_SB_STATUS_NTFY_DESC
dwOutBufSize – [in] Size of the output buffer in bytes
pdwNumOutData – [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer.
- Returns:
EC_E_NOERROR or error code
See also
6.16.4. emIoCtl - EC_IOCTL_SB_SET_TOPOLOGY_CHANGED_DELAY
-
EC_IOCTL_SB_SET_TOPOLOGY_CHANGED_DELAY
Set the topology changed delay value. The master will wait this duration [ms] to react on appearing links in topology. The default value is 1000 ms.
- Parameters:
pbyInBuf – [in] Pointer to EC_T_DWORD containing the delay information [ms]
dwInBufSize – [in] Size of the input buffer provided at pbyInBuf in bytes
pbyOutBuf – [out] Should be set to EC_NULL
dwOutBufSize – [in] Should be set to 0
pdwNumOutData – [out] Should be set to EC_NULL
- Returns:
EC_E_NOERROR or error code
6.16.5. emIoCtl - EC_IOCTL_SB_SET_TOPOLOGY_CHANGED_DELAYS
-
EC_IOCTL_SB_SET_TOPOLOGY_CHANGED_DELAYS
Set the topology changed delay values individually. The master will wait individual durations [ms] (0 ms: disabled) for slave ports, main link and red link to react on appearing links in topology. The default value is 1000 ms.
- Parameters:
pbyInBuf – [in] Pointer to EC_T_TOPOLOGY_CHANGED_DELAYS containing the delay durations [ms]
dwInBufSize – [in] Size of the input buffer provided at pbyInBuf in bytes
pbyOutBuf – [out] Should be set to EC_NULL
dwOutBufSize – [in] Should be set to 0
pdwNumOutData – [out] Should be set to EC_NULL
- Returns:
EC_E_NOERROR or error code
-
struct EC_T_TOPOLOGY_CHANGED_DELAYS
Public Members
-
EC_T_DWORD dwSlavePort
[in] Delay before opening slave port after link connection detected
-
EC_T_DWORD dwMainLine
[in] Delay before sending frames at main line after link connection detected
-
EC_T_DWORD dwRedLine
[in] Delay before sending frames at red line after link connection detected
-
EC_T_DWORD adwReserved[5]
reserved
-
EC_T_DWORD dwSlavePort
6.16.6. emIoCtl - EC_IOCTL_SB_SET_ERROR_ON_CROSSED_LINES
-
EC_IOCTL_SB_SET_ERROR_ON_CROSSED_LINES
Enable or disable bus mismatch if IN and OUT connectors are swapped. If enabled the swapped IN and OUT connectors will lead to bus mismatch. By default swapped IN and OUT connectors will lead to bus mismatch.
- Parameters:
pbyInBuf – [in] Pointer to EC_T_BOOL variable. If set to EC_TRUE swapped IN and OUT connectors will lead to bus mismatch, if set to EC_FALSE swapped IN and OUT connectors are tolerated.
dwInBufSize – [in] Size of the input buffer provided at pbyInBuf in bytes
pbyOutBuf – [out] Should be set to EC_NULL
dwOutBufSize – [in] Should be set to 0
pdwNumOutData – [out] Should be set to EC_NULL
- Returns:
EC_E_NOERROR or error code
6.16.7. emIoCtl - EC_IOCTL_SB_SET_ERROR_ON_LINE_BREAK
-
EC_IOCTL_SB_SET_ERROR_ON_LINE_BREAK
Enable or disable bus mismatch if a line is broken in a redundant network. If enabled, line breaks in cable or junction redundant networks will lead to bus mismatch.
Note
EC_E_REDLINEBREAK: Line break in a cable redundant network.
Note
EC_E_JUNCTION_RED_LINE_BREAK: Line break in a junction redundant network.
Note
See EC_NOTIFY_SB_MISMATCH, EC_NOTIFY_SB_STATUS.
- Parameters:
pbyInBuf – [in] Pointer to value of EC_T_BOOL: EC_TRUE: Enable, EC_FALSE: Disable. Default: Enabled.
dwInBufSize – [in] Should be set to sizeof(EC_T_BOOL)
pbyOutBuf – [out] Should be set to EC_NULL
dwOutBufSize – [in] Should be set to 0
pdwNumOutData – [out] Should be set to EC_NULL
- Returns:
EC_E_NOERROR or error code
6.16.8. emIoCtl - EC_IOCTL_SB_SET_TOPOLOGY_CHANGE_AUTO_MODE
Warning
This documentation is preliminary and is subject to change
-
EC_IOCTL_SB_SET_TOPOLOGY_CHANGE_AUTO_MODE
Enable or disable the automatic topology change mode. By default the automatic mode is enabled.
- Parameters:
pbyInBuf – [in] Pointer to EC_T_BOOL variable. If set to EC_TRUE the automatic mode is enabled.
dwInBufSize – [in] Size of the input buffer provided at pbyInBuf in bytes
pbyOutBuf – [out] Should be set to EC_NULL
dwOutBufSize – [in] Should be set to 0
pdwNumOutData – [out] Should be set to EC_NULL
- Returns:
EC_E_NOERROR or error code
In automatic mode, new SubDevices will be discovered automatically. In manual mode, after new SubDevices have been connected, an emNotify - EC_NOTIFY_HC_TOPOCHGDONE notification will be given without opening the ports of the SubDevices on the bus. When the application is able to handle the new SubDevices, it should call emIoCtl - EC_IOCTL_SB_ACCEPT_TOPOLOGY_CHANGE.
6.16.9. emIoCtl - EC_IOCTL_SB_ACCEPT_TOPOLOGY_CHANGE
Warning
This documentation is preliminary and is subject to change
-
EC_IOCTL_SB_ACCEPT_TOPOLOGY_CHANGE
This call will trigger a scan bus for accept topology change (manual mode). On completion the Notfication EC_NOTIFY_SB_STATUS is given.
- Parameters:
pbyInBuf – [in] Should be set to EC_NULL
dwInBufSize – [in] Should be set to 0
pbyOutBuf – [out] Should be set to EC_NULL
dwOutBufSize – [in] Should be set to 0
pdwNumOutData – [out] Should be set to EC_NULL
- Returns:
EC_E_NOERROR or error code
This function may be called after an emNotify - EC_NOTIFY_HC_TOPOCHGDONE notification was given if the automatic topology change mode was previously disabled using emIoCtl - EC_IOCTL_SB_SET_TOPOLOGY_CHANGE_AUTO_MODE.
During this bus scan the ports of the SubDevices will (re)open and new SubDevices can be detected.
The timeout value given by emIoCtl - EC_IOCTL_SB_ENABLE will be used. When issuing this IoCtl, the application has to take care emExecJob() is called cyclically to trigger MainDevice state machines, timers, send acyc and receive frames accordingly.
6.16.10. emNotify - EC_NOTIFY_SB_STATUS
Bus scan status notification.
This notification is enabled by default.
- emNotify - EC_NOTIFY_SB_STATUS
- Parameter
pbyInBuf: [in] Pointer to EC_T_SB_STATUS_NTFY_DESCdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
-
struct EC_T_SB_STATUS_NTFY_DESC
Public Members
-
EC_T_DWORD dwResultCode
[in] EC_E_NOERROR: success, EC_E_NOTREADY: no bus scan executed, EC_E_BUSCONFIG_MISMATCH: bus configuration mismatch result of scanbus
-
EC_T_DWORD dwSlaveCount
[in] Number of slaves connected to the bus
-
EC_T_DWORD dwResultCode
See also
emIoCtl - EC_IOCTL_SET_NOTIFICATION_ENABLED for how to control the deactivation
6.16.11. emNotify - EC_NOTIFY_SB_MISMATCH
This notification will be initiated if a bus scan detects a mismatch of connected SubDevices and configuration, due to unexpected SubDevices or missing mandatory SubDevices.
- emNotify - EC_NOTIFY_SB_MISMATCH
- Parameter
pbyInBuf: [in] Pointer to EC_T_SB_MISMATCH_DESCdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
This notification is enabled by default. In case of permanent frame loss no SubDevices can be found although the SubDevices are connected.
-
struct EC_T_SB_MISMATCH_DESC
Public Members
-
EC_T_WORD wPrevFixedAddress
[in] Previous slave station address
-
EC_T_WORD wPrevPort
[in] Previous slave station address
-
EC_T_WORD wPrevAIncAddress
[in] Previous slave auto-increment address
-
EC_T_WORD wBusAIncAddress
[in] Unexpected slave (bus) auto-inc address
-
EC_T_DWORD dwBusVendorId
[in] Unexpected slave (bus) vendor ID
-
EC_T_DWORD dwBusProdCode
[in] Unexpected slave (bus) product code
-
EC_T_DWORD dwBusRevisionNo
[in] Unexpected slave (bus) revision number
-
EC_T_DWORD dwBusSerialNo
[in] Unexpected slave (bus) serial number
-
EC_T_WORD wBusFixedAddress
[in] Unexpected slave (bus) station address
-
EC_T_BOOL bIdentificationError
[in] Identification command sent to slave but failed
-
EC_T_WORD wIdentificationAdo
[in] Identification register
-
EC_T_WORD wIdentificationVal
[in] Last identification value read from slave according to the last used identification method
-
EC_T_WORD wIdentificationValExpected
[in] Identification expected value
-
EC_T_WORD wCfgFixedAddress
[in] Missing slave (config) station Address
-
EC_T_WORD wCfgAIncAddress
[in] Missing slave (config) Auto-Increment Address
-
EC_T_DWORD dwCfgVendorId
[in] Missing slave (config) Vendor ID
-
EC_T_DWORD dwCfgProdCode
[in] Missing slave (config) Product code
-
EC_T_DWORD dwCfgRevisionNo
[in] Missing slave (config) Revision Number
-
EC_T_DWORD dwCfgSerialNo
[in] Missing slave (config) Serial Number
-
EC_T_WORD wPrevFixedAddress
See also
emIoCtl - EC_IOCTL_SET_NOTIFICATION_ENABLED for how to control the deactivation
6.16.12. emNotify - EC_NOTIFY_SB_DUPLICATE_HC_NODE
A bus mismatch was detected during the scan due to duplicated SubDevice(s). The application receives this notification if there are two SubDevices on the network with the same product code, vendor ID and identification value (alias address or switch id).
- emNotify - EC_NOTIFY_SB_DUPLICATE_HC_NODE
- Parameter
pbyInBuf: [in] Pointer to EC_T_SB_MISMATCH_DESCdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The members of EC_T_SB_MISMATCH_DESC have the following meaning:
EC_T_SB_MISMATCH_DESC::wCfgFixedAddressDuplicated SubDevice (config) station AddressEC_T_SB_MISMATCH_DESC::wCfgAIncAddressDuplicated SubDevice (config) Auto-Increment Address.EC_T_SB_MISMATCH_DESC::dwCfgVendorIdDuplicated SubDevice (config) Vendor IDEC_T_SB_MISMATCH_DESC::dwCfgProdCodeDuplicated SubDevice (config) Product codeEC_T_SB_MISMATCH_DESC::dwCfgRevisionNoDuplicated SubDevice (config) Revision NumberEC_T_SB_MISMATCH_DESC::dwCfgSerialNoDuplicated SubDevice (config) Serial Number
6.16.13. emNotify - EC_NOTIFY_SLAVE_PRESENCE
This notification is given when a SubDevice appears or disappears from the network.
This notification is enabled by default.
- emNotify - EC_NOTIFY_SLAVE_PRESENCE
- Parameter
pbyInBuf: [in] Pointer to EC_T_SLAVE_PRESENCE_NTFY_DESCdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
Disconnecting the SubDevice from the network, powering it off or a bad connection can produce this notification.
See also
emIoCtl - EC_IOCTL_SET_NOTIFICATION_ENABLED for how to control the deactivation
6.16.14. emNotify - EC_NOTIFY_SLAVES_PRESENCE
This notification collects notifications of the type emNotify - EC_NOTIFY_SLAVE_PRESENCE. Notification is given either upon completion or when the MainDevice status is changed, whichever comes first. Disconnecting SubDevices from the network, turning them off, or having a bad connection can lead to this notification.
This notification is disabled by default.
- emNotify - EC_NOTIFY_SLAVES_PRESENCE
- Parameter
pbyInBuf: [in] Pointer to EC_T_SLAVES_PRESENCE_NTFY_DESCdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
-
struct EC_T_SLAVES_PRESENCE_NTFY_DESC
Public Members
-
EC_T_WORD wCount
Number of slave presence notifications
-
EC_T_SLAVE_PRESENCE_NTFY_DESC SlavePresence[MAX_SLAVES_PRESENCE_NTFY_ENTRIES]
Slave presence descriptions
-
EC_T_WORD wCount
6.16.15. emNotify - EC_NOTIFY_LINE_CROSSED
Cable swapping detected. All SubDevice’s port 0 must lead to MainDevice.
- emNotify - EC_NOTIFY_LINE_CROSSED
- Parameter
pbyInBuf: [in] Pointer to EC_T_LINE_CROSSED_DESCdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
-
struct EC_T_LINE_CROSSED_DESC
Public Members
-
EC_T_SLAVE_PROP SlaveProp
Slave properties
-
EC_T_WORD wInputPort
Port where frame was received
-
EC_T_SLAVE_PROP SlaveProp
6.16.16. emNotify - EC_NOTIFY_SLAVE_NOTSUPPORTED
Is currently generated during Bus Scan if emConfigureNetwork() (GenOp/Preop) and a wrong category type is detected in the EEPROM. This notification should only print a log message or be ignored (EC-Master print log message itself).
- emNotify - EC_NOTIFY_SLAVE_NOTSUPPORTED
- Parameter
pbyInBuf: [in] Pointer to EC_T_ERROR_NOTIFICATION_DESC containing EC_T_SLAVE_NOTSUPPORTED_DESCdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
-
struct EC_T_SLAVE_NOTSUPPORTED_DESC
Public Members
-
EC_T_SLAVE_PROP SlaveProp
Slave properties
-
EC_T_SLAVE_PROP SlaveProp
6.16.17. emNotify - EC_NOTIFY_FRAMELOSS_AFTER_SLAVE
Is currently generated and automatically handled during emRescueScan() if opening a port would lead to frame loss. This notification should only print a log message.
- emNotify - EC_NOTIFY_FRAMELOSS_AFTER_SLAVE
- Parameter
pbyInBuf: [in] Pointer to EC_T_ERROR_NOTIFICATION_DESC containing EC_T_FRAMELOSS_AFTER_SLAVE_NTFY_DESCdwInBufSize: [in] Size of the input buffer provided at pbyInBuf in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
6.16.18. emNotify - Bus Scan notifications for Feature Packs
The notifications EC_NOTIFY_RED_LINEBRK, EC_NOTIFY_RED_LINEFIXED belong to the Feature Pack Redundancy.
The notifications EC_NOTIFY_HC_DETECTADDGROUPS, EC_NOTIFY_HC_PROBEALLGROUPS belong to the Feature Pack Hot Connect.
6.16.19. emIoCtl - EC_IOCTL_SB_NOTIFY_UNEXPECTED_BUS_SLAVES
-
EC_IOCTL_SB_NOTIFY_UNEXPECTED_BUS_SLAVES
Enable or disable unexpected bus slaves notification.
- Parameters:
pbyInBuf – [in] Pointer to EC_T_BOOL variable. If set to EC_TRUE unexpected bus slaves on the network will be notified by EC_NOTIFY_SB_MISMATCH.
dwInBufSize – [in] Size of the input buffer provided at pbyInBuf in bytes
pbyOutBuf – [out] Should be set to EC_NULL
dwOutBufSize – [in] Should be set to 0
pdwNumOutData – [out] Should be set to EC_NULL
- Returns:
EC_E_NOERROR or error code
6.16.20. emIsTopologyChangeDetected
-
static EC_T_DWORD ecatIsTopologyChangeDetected(EC_T_BOOL *pbTopologyChangeDetected)
-
EC_T_DWORD emIsTopologyChangeDetected(EC_T_DWORD dwInstanceID, EC_T_BOOL *pbTopologyChangeDetected)
Returns whether topology change detected.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pbTopologyChangeDetected – [out] Pointer to EC_T_BOOL value: EC_TRUE if Topology Change Detected, EC_FALSE if not
- Returns:
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if EtherCAT stack isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range
EC_E_MASTER_RED_STATE_INACTIVE if Master Redundancy is configured and master is inactive
6.16.21. emNotify - EC_NOTIFY_HC_TOPOCHGDONE
This notification is raised when a topology change was completely processed.
- emNotify - EC_NOTIFY_HC_TOPOCHGDONE
- Parameter
pbyInBuf: [in] Pointer to EC_T_DWORD (EC_E_NOERROR on success, Error code otherwise)dwInBufSize: [in] sizeof(EC_T_DWORD)pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The notification is raised when the SubDevices have been detected and DC initialized.
6.16.22. emIoCtl - EC_IOCTL_SB_SET_NO_DC_SLAVES_AFTER_JUNCTION
-
EC_IOCTL_SB_SET_NO_DC_SLAVES_AFTER_JUNCTION
Declares that no DC slaves are located after junction.
- Parameters:
pbyInBuf – [in] Pointer to EC_T_BOOL variable. If set to EC_TRUE the hidden slave detection and the junction redundancy specific propagation delay measurement are not executed.
dwInBufSize – [in] Size of the input buffer provided at pbyInBuf in bytes
pbyOutBuf – [out] Should be set to EC_NULL
dwOutBufSize – [in] Should be set to 0
pdwNumOutData – [out] Should be set to EC_NULL
- Returns:
EC_E_NOERROR or error code
Calling this IOCTL if DC SubDevices are located in or after a junction redundancy segment will generate an undefined behavior.