7.1. Integration Requirements
To use the diagnosis tool EC-Lyser with a customer application, some modifications have to be done during integration of the EC-Master. The task is to integrate and start the Remote API Server system within the custom application, which provides a socket based uplink, which later on is connected by the EC-Lyser.
An example on how to integrate the Remote API Server within the application is given with the example application EcMasterDemo, which in case is pre-configured to listen for EC-Lyser on TCP Port 6000 when command line parameter EcMasterDemo -sp is given.
To clarify the steps which are needed within a custom application, a developer may use the following pseudo-code segment as a point of start. The Remote API Server library EcMasterRasServer.lib (or respectively EcMasterRasServer.a) must be linked.