1. Introduction
1.1. What is EtherCAT®?
EtherCAT® (Ethernet for Control Automation Technology) is a high-performance Ethernet Fieldbus technology that provides a reliable, efficient, and cost-effective communication solution for a wide variety of industrial automation applications. Originally developed as an open technology by Beckhoff Automation in 2003, and subsequently turned over to an independent organization known as the EtherCAT® Technology Group, EtherCAT® has since become one of the most widely used industrial Ethernet protocols in the world.
See also
A comprehensive introduction to EtherCAT® technology can be found at https://www.acontis.com/en/what-is-ethercat-communication-protocol.html.
1.2. The EC-Master - Features
Feature ID: Unique identification used in ETG.1500 EtherCAT MainDevice Classes
- 1(1,2,3)
: According to ETG.1500 MainDevice Classes not mandatory for Class A
- 2(1,2,3,4,5,6,7,8,9)
: According to ETG.1500 MainDevice Classes not mandatory for Class B
Feature name |
Short description |
EC-Master Class A |
EC-Master Class B |
Feature ID |
|---|---|---|---|---|
Basic Features |
||||
Service Commands |
Support of all commands |
✅ |
✅ |
101 |
IRQ field in datagram |
Use IRQ information from SubDevice in datagram header |
✅ |
✅ |
102 |
SubDevices with Device Emulation |
Support SubDevices with and without application controller |
✅ |
✅ |
103 |
EtherCAT® State Machine |
Support of ESM special behavior |
✅ |
✅ |
104 |
Error Handling |
Checking of network or SubDevice errors, e.g. Working Counter |
✅ |
✅ |
105 |
VLAN |
Support VLAN Tagging |
✅ |
106 |
|
EtherCAT® Frame Types |
Support EtherCAT® Frames |
✅ |
✅ |
107 |
UDP Frame Types |
Support UDP Frames |
108 |
||
Process Data Exchange |
||||
Cyclic PDO |
Cyclic process data exchange |
✅ |
✅ |
201 |
Multiple Tasks |
Different cycle tasks Multiple update rates for PDO |
✅ |
✅ |
202 |
Frame repetition |
Send cyclic frames multiple times to increase immunity |
203 |
||
Network Configuration |
||||
Online scanning |
Network configuration functionality included in EtherCAT® MainDevice |
✅ |
✅ |
301 |
Reading ENI |
Network Configuration taken from ENI file |
✅ |
✅ |
301 |
Compare Network configuration |
Compare configured and existing network configuration during boot-up |
✅ |
✅ |
302 |
Explicit Device ID |
Identification used for Hot Connect and prevention against cable swapping |
✅ |
✅ |
303 |
Station Alias Addressing |
Support configured station alias in SubDevice, i.e. enable 2nd Address and use it |
✅ |
✅ |
304 |
Access to EEPROM |
Support routines to access EEPROM via ESC register |
✅ |
✅ |
305 |
Mailbox Support |
||||
Support Mailbox |
Main functionality for mailbox transfer |
✅ |
✅ |
401 |
Mailbox Resilient Layer |
Support underlying resilient layer |
✅ |
✅ |
402 |
Multiple Mailbox channels |
✅ |
✅ |
403 |
|
Mailbox polling |
Polling Mailbox state in SubDevices |
✅ |
✅ |
404 |
CAN application layer over |ETHERCAT_R| (CoE) |
||||
SDO Up/Download |
Normal and expedited transfer |
✅ |
✅ |
501 |
Segmented Transfer |
Segmented transfer |
✅ |
✅ |
502 |
Complete Access |
Transfer the entire object (with all subindices) at once |
✅ |
✅ |
503 |
SDO Info service |
Services to read object dictionary |
✅ |
✅ |
504 |
Emergency Message |
Receive Emergency messages |
✅ |
✅ |
505 |
PDO in CoE |
PDO services transmitted via CoE |
506 |
||
EoE |
||||
EoE protocol |
Services for tunneling Ethernet frames. includes all specified EoE services |
✅ |
✅ |
601 |
Virtual Switch |
Virtual Switch functionality |
✅ |
✅ |
602 |
EoE Endpoint to Operation Systems |
Interface to the Operation System on top of the EoE layer |
FP |
603 |
|
FoE |
||||
FoE Protocol |
Support FoE Protocol |
✅ |
✅ |
701 |
Firmware Up-/Download |
Password, FileName should be given by the application |
✅ |
✅ |
702 |
Boot State |
Support Boot-State for Firmware Up/Download |
✅ |
✅ |
703 |
SoE |
||||
SoE Protocol |
Support SoE Services |
✅ |
✅ |
801 |
AoE |
||||
AoE Protocol |
Support AoE Protocol |
✅ |
✅ |
901 |
VoE |
||||
VoE Protocol |
External Connectivity supported |
✅ |
✅ |
1001 |
Synchronization with Distributed Clock (DC) |
||||
DC support |
Support of Distributed Clocks |
✅ |
1101 |
|
Continuous Propagation Delay compensation |
Continuous Calculation of the propagation delay |
✅ |
1102 |
|
Sync window monitoring |
Continuous monitoring of the Synchronization difference between SubDevices |
✅ |
1103 |
|
SubDevice-to-SubDevice Communication |
||||
via MainDevice |
Information is given in ENI file or can be part of any other network configuration. Copying of the data can be handled by MainDevice stack or MainDevice’s application |
✅ |
✅ |
1201 |
MainDevice information |
||||
MainDevice Object Dictionary |
FP |
1301 |
1.3. Protected version
The EC-Master software can be delivered in 3 different versions:
- Protected
Binary with MAC protection
- Unrestricted
Binary without MAC protection
- Dongled
Encrypted binary
The protected version will automatically stop after about 1 hour of continuous operation. In order to remove this restriction a valid runtime license key is required. The runtime license protection is based on the MAC address of the Ethernet controller used for the EtherCAT® protocol. With a valid License Key the protected version of EC-Master will automatically become an unrestricted version.
1.3.1. Licensing procedure for Development Licenses
Installation of EC-Master protected version
Determine the MAC Address by calling
emGetSrcMacAddress()or from a sticker applied on the hardware near the Ethernet controllerSend an Email with the subject “Development License Key Request, Commission your commission number” with the MAC address to sales@acontis.com
Acontis will create the license keys and return them in a License Key Text File (CSV format).
Number;MAC Address;License Key 1;00-00-5A-11-77-FE;DA1099F2-15C249E9-54327FBC 2;64-31-50-80-20-4E;1B7C1F86-D08E40A8-4F96F2BA 3;2C-F0-5D-03-CB-2B;10005078-DFD9A2C3-5FD4B1CD-35041597-F8094AA4-6C7CCE7E
Activate the License Key by calling
emSetLicenseKey()with the license key that corresponds to the MAC address on the hardware and check the return code. The license key is 26 or 53 characters long.dwRes = emSetLicenseKey(0, "DA1099F2-15C249E9-54327FBC");
1.3.2. Licensing procedure for Runtime Licenses
Installation of EC-Master protected version
Determine the MAC Address by calling
emGetSrcMacAddress()or from a sticker applied on the hardware near the Ethernet controllerProvide the MAC Addresses and numbers from previously ordered and unused runtime license stickers in a text file to acontis as described in the example below. Please use a separate line for each runtime license sticker number and MAC Address.
S/N; MAC Address 100-105-1-1/1603310001;00-00-5A-11-77-FE 100-105-1-1/1603310002;64-31-50-80-20-4E 100-105-1-1/1603310003;2C-F0-5D-03-CB-2B
Send an Email with the subject “Runtime License Key Request, Commission your commission number” with the MAC address to sales@acontis.com
Acontis will create the license keys and return them in a License Key Text File.
Number;MAC Address;License Key 1;00-00-5A-11-77-FE;DA1099F2-15C249E9-54327FBC 2;64-31-50-80-20-4E;1B7C1F86-D08E40A8-4F96F2BA 3;2C-F0-5D-03-CB-2B;10005078-DFD9A2C3-5FD4B1CD-35041597-F8094AA4-6C7CCE7E
Activate the License Key by calling
emSetLicenseKey()with the license key that corresponds to the MAC address on the hardware and check the return code.dwRes = emSetLicenseKey(0, "DA1099F2-15C249E9-54327FBC");
1.4. Dongled version
The Master library is encrypted and requires a dongle to execute. The following dongles are supported:
USB dongle
ASIC dongle
Virtual dongle using a WibuCmRaU file
1.4.1. Licensing using a virtual WibuCmRaU File on Linux
To create a virtual dongle using a WibuCmRaU file on a Linux machine, the following steps are required:
Download the codemeter package from Wibu website and install it on the linux machine:
- Import the LIF file provided by acontis
cmu --import --file *.WibuCmLIF
- List the Wibu licenses, to get the serial number
cmu --list
- Use the serial number to generate a WibuCmRaC file
cmu --serial your_serial_number --context 6001978 --file *.WibuCmRaC
Send the WibuCmRaC to acontis and acontis will provide a WibuCmRaU file.
- Import the WibuCmRaU file
cmu --import --file *.WibuCmRaU
1.4.2. Maintain the license after a linux image update
In case of a complete Linux image update, the following steps are required:
Make a backup of the WibuCmRaU file and the following folder /var/lib/Codemeter/CmAct from the old image.
On the new image install Codemeter
Restore the 6001978_* files from /var/lib/Codemeter/CmAct
- Change the user rights of the 4 files to daemon
sudo chown daemon:daemon 6001978_*
- Import the WibuCmRaU backup file
cmu --import --file *.WibuCmRaU
1.5. License
1.5.1. EC-Master license
According to EC-Master Software License Agreement (SLA).
1.5.2. Free Open Source Software contained in EC-Master
1.5.2.1. Expat XML parser license V2.6.0
Copyright (c) 1997-2000 Thai Open Source Software Center Ltd
Copyright (c) 2000 Clark Cooper <coopercc@users.sourceforge.net>
Copyright (c) 2000-2005 Fred L. Drake, Jr. <fdrake@users.sourceforge.net>
Copyright (c) 2001-2002 Greg Stein <gstein@users.sourceforge.net>
Copyright (c) 2002-2016 Karl Waclawek <karl@waclawek.net>
Copyright (c) 2016-2024 Sebastian Pipping <sebastian@pipping.org>
Copyright (c) 2016 Cristian Rodríguez <crrodriguez@opensuse.org>
Copyright (c) 2016 Thomas Beutlich <tc@tbeu.de>
Copyright (c) 2017 Rhodri James <rhodri@wildebeest.org.uk>
Copyright (c) 2022 Thijs Schreijer <thijs@thijsschreijer.nl>
Copyright (c) 2023 Hanno Böck <hanno@gentoo.org>
Copyright (c) 2023 Sony Corporation / Snild Dolkow <snild@sony.com>
Licensed under the MIT license:
Permission is hereby granted, free of charge, to any person obtaining
a copy of this software and associated documentation files (the
"Software"), to deal in the Software without restriction, including
without limitation the rights to use, copy, modify, merge, publish,
distribute, sublicense, and/or sell copies of the Software, and to permit
persons to whom the Software is furnished to do so, subject to the
following conditions:
The above copyright notice and this permission notice shall be included
in all copies or substantial portions of the Software.
THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND,
EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF
MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN
NO EVENT SHALL THE AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM,
DAMAGES OR OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR
OTHERWISE, ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE
USE OR OTHER DEALINGS IN THE SOFTWARE.
1.5.3. Free Open Source Software supported by EC-Master
The following components are not part of EC-Master, but relate to it:
1.5.3.1. acontis atemsys Linux kernel module
The acontis atemsys is licensed under the GPL:
Copyright (c) 2009 - 2020 acontis technologies GmbH, Ravensburg, Germany
All rights reserved.
This program is free software; you can redistribute it and/or modify it
under the terms of the GNU General Public License as published by the
Free Software Foundation; either version 2 of the License, or (at your
option) any later version.
1.6. Versioning
EC-Master follows the following versioning scheme: VMAJOR. MINOR. SERVICEPACK. BUILD (e.g. V3.2.1.04).
The libraries are binary compatible by unchanged MAJOR and MINOR digits. If SERVICEPACK increments, BUILD restarts with 01. BUILD 99 is reserved for test builds that have not been officially released for productive usage.