Texas Instruments ICSSG - emllICSSG on AM654x

5.20. Texas Instruments ICSSG - emllICSSG on AM654x

The parameters to the ICSSG Real-time Ethernet Driver are setup-specific. The function CreateLinkParmsFromCmdLineICSSG() in EcSelectLinkLayer.cpp demonstrates how to initialize the Real-time Ethernet Driver instance.

Public Members

Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_ICSSG.

TI System on Chip board type

Initialize whole PRUSS subsystem, not only port. This flag is always required when the link layer is used on a single ICSSG port. This flag is also required, when the link layer is used in “Redundancy mode” and two ICSSG ports are used. In this case, first port should be master, and second port should be slave.

Values:

TI AM654x

5.20.1. TI AM654x IDK

Support for ICSSG on AM654x is currently limited to TI AM654x IDK/EVK with TI RTOS/Sysbios in polling mode.