2. Getting Started
2.1. EC-Master Architecture
The EC-Master EtherCAT® MainDevice stack is implemented in C++ and can be easily ported to any embedded OS platforms using an appropriate C++ compiler. The API functions are C language interfaces, thus the MainDevice stack can be used in ANSI-C as well as in C++ environments.
The MainDevice stack is divided into modules, see diagram and descriptions below:
EtherCAT® MainDevice Core: In the core module cyclic (process data update) and acyclic (mailbox) EtherCAT® commands are sent and received. Among others there exist some state machines to handle for example the mailbox protocols.
Configuration Layer: The EtherCAT® MainDevice is configured using an XML file whose format is fixed in the EtherCAT® specification ETG.2100. EC-Master contains an OS independent XML parser.
Real-time Ethernet Driver Layer: This layer exchanges Ethernet frames between the MainDevice and the SubDevices. If hard real-time requirements exist, this layer has to be optimized for the network adapter card in use.
OS Layer: All OS dependent system calls are encapsulated in a small OS layer. Most functions are that easy that they can be implemented using simple C macros.
2.2. EtherCAT® Network Configuration (ENI)
The EtherCAT® MainDevice has to know about the EtherCAT® bus topology and the cyclic/acyclic frames to exchange with the SubDevices. This configuration is determined in a configuration file which has to be available in the EtherCAT® Network Information Format (ENI). This format is completely independent from EtherCAT® SubDevice vendors, from EtherCAT® MainDevice vendors and from EtherCAT® configuration tools. Thus interoperability between those vendors is guaranteed.
Additionally some static configuration parameters have to be defined like the identification of the network adapter card to use, the priority of the EtherCAT® MainDevice timer task etc.
2.3. Operating system configuration
The main task is to setup the operating system to support the appropriate network adapter for EtherCAT® usage and for some systems real-time configuration may be needed.
The operating system-specific settings and configurations are described in Platform and Operating Systems (OS).
2.4. Running EcMasterDemo
The EcMasterDemo is available “out of the box” for different operating systems. It is an EC-Master example application that handles the following tasks:
Showing basic EtherCAT® communication
MainDevice stack initialization into OPERATIONAL state
Process Data operations for e.g. Beckhoff EL2004, EL1004 and EL4132
Periodic diagnosis task
Periodic Job Task in polling mode
Logging
Start the EcMasterDemo from the command line to put the EtherCAT® network into operation. At least a Real-time Ethernet Driver must be specified.
EcMasterDemo -ndis 192.168.157.2 1 -f eni.xml -t 0 -v 3
See also
Example application for detailed explanation
2.4.1. Command line parameters
- EcMasterDemo <LinkLayer> [-f ENI-FileName] [-t time] [-b cycle time] [-a affinity] [-v level] [-perf [level]] [-log prefix [msg cnt]] [-lic key] [-oem key] [-maxbusslaves cnt] [-flash address] [-sp [port]] [-rec [prefix [frame cnt]]] [-junctionred]
The parameters are as follows:
- -t <time>
Running duration [ms]. When the time expires the demo application exits completely.
- <time>
Time [ms], 0 = forever (default = 120000)
- -b <cycle time>
Specifies the bus cycle time. Defaults to 1000 µs (1 ms).
- <cycle time>
Bus cycle time in µsec
- -a <affinity>
The CPU affinity specifies which CPU the demo application ought to use.
- <affinity>
0 = first CPU, 1 = second, …
- -v <level>
The verbosity level specifies how much console output messages will be generated by the demo application. A high verbosity level leads to more messages.
- <level>
Verbosity level: 0=off (default), 1..n=more messages
- -perf [<level>]
Enable max. and average time measurement in µs for all EtherCAT® jobs (e.g. ProcessAllRxFrames).
- <level>
Depending on level the performance histogram can be activated as well.
- -log <prefix> [<msg cnt>]
Use given file name prefix for log files.
- <prefix>
- <msg cnt>
Messages count for log buffer allocation
- -sp [<port>]
If platform has support for IP Sockets, this command-line option enables the Remote API Server to be started. The Remote API Server is going to listen on TCP Port 6000 (or port parameter if given) and is available for connecting Remote API Clients.
- <port>
RAS server port
- -rec [<prefix> [<frame cnt>]]
Packet capture file recording
- <prefix>
File name prefix
- <frame cnt>
Frame count for log buffer allocation
2.4.1.1. Link Layer
Using one of the following demo application Link Layer options, the EC-Master will dynamically load the network driver for the specified network adapter card and use the appropriate network driver to access the Ethernet adapter for EtherCAT®.
ShowSyntaxLinkLayer() in Common/EcSelectLinkLayer.cpp is called automatically if the Demo application is started without parameters and lists the possibilities.
Note
Not all link layers are available on all operating systems or architectures. A detailed view in the form of a matrix can be found in the developer center.
- -alteratse <instance> <mode>
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- -bcmgenet <instance> <mode>
- Hardware: Broadcom BcmGenet
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- -bcmnetxtreme <instance> <mode>
- Hardware: Broadcom NetXtreme
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- -bpf <instance> <mode> <interface> [<prefix>]
- Hardware: Berkeley Packet Filter, Hardware independent
- <Instance>
BPF instance (0=first), results to e.g. /dev/bpf0
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- <Interface>
Name of Ethernet Interface, e.g. wm0
- Optional:
- <Prefix>
Prefix of the BPF instance path, e.g. /alt
- -ccat <instance> <mode>
- Hardware: Beckhoff CCAT
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- -cpsw <instance> <mode> <portpriority> <masterflag> <refboard>
- Hardware: TI CPSW
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode, 1 = Polling mode
- <PortPriority>
Low priority (0) or high priority (1)
- <MasterFlag>
(m) Master (Initialize Switch), (s) Slave
- <RefBoard>
bone | am3359-icev2 | am437x-idk | am572x-idk | 387X_evm | custom | osdriver
- If custom:
- <CpswType>
am33XX | am437X | am57X | am387X
- <PhyAddress>
0 … 31
- <PhyInterface>
rmii | gmii | rgmii | osdriver
- <NotUseDmaBuffers>
0 = FALSE | 1 = TRUE
- -dpdk <instance> <mode> <port>
- Hardware: Hardware independent, only available for Linux.
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode (not implemented), 1 = Polling mode
- <Port>
DPDK port ID, e.g. 0
This option supports a large variety of NICs. Whether a NIC is supported depends on its network driver. For a list of supported network drivers see https://www.dpdk.org.
- -dpdkenetc4 <instance> <mode> <port>
- Hardware: NXP iMX95 ENETC4, only available for Linux.
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode (not implemented), 1 = Polling mode
- <Port>
DPDK port ID, e.g. 0
- -dw3504 <instance> <mode> <refboard>
- Hardware: Synopsys DesignWare 3504-0 Universal 10/100/1000 Ethernet MAC (DW3504)
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- <RefBoard>
Reference Board: intel_atom | lces1 | rd55up06 | r12ccpu | rzn1 | socrates | stm32mp157a-dk1 | custom
- If custom:
- <DW3504Type>
intel_atom | cycloneV | lces1 | stm32mp157a-dk1
- <PhyInterface>
fixed | mii | rmii | gmii | sgmii | rgmii | osdriver
- <PhyAddress>
0 … 31 (don’t use if osdriver)
- -dwxgmac <instance> <mode> <RefBoard>
- Hardware: Synopsys DesignWare Cores XGMAC 10G/25G Ethernet MAC
- <instance>
Device instance 1 = first, 2 = second, …
- <mode>
0 = Interrupt mode | 1 = Polling mode
- <RefBoard>
Reference Board: jetson-agx-orin | jetson-agx-thor
- -eg20t <instance> <mode>
- Hardware: Intel EG20T Gigabit Ethernet Controller
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- -emac <instance> <mode> <refboard>
- Hardware: Xilinx LogiCORE IP XPS EMAC
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- <RefBoard>
MC2002E | custom
- If custom:
- <RegisterBase>
Register base address as hex value
- <RegisterLength>
Register length as hex value
- <NotUseDmaBuffers>
0 = FALSE | 1 = TRUE
- -fslenetc <instance> <mode> <refboard>
- Hardware: NXP ENETC4 (NETC, i.MX95)
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
1 = Polling mode
- <RefBoard>
verdin-imx95 | custom
- If custom:
- <Type>
imx95
- <PhyInterface>
fixed | osdriver
- <PhyAddress>
0 … 31 (ignored if osdriver)
- -fsletsec <instance> <mode> <refboard>
- Hardware: Freescale TSEC / eTSEC V1 / eTSEC V2 (VeTSEC)
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- <RefBoard>
p2020rdb | twrp1025 | istmpc8548 | xj_epu20c | twrls1021a | tqmls_ls102xa | custom
- If custom:
- <PhyAddress>
0 … 31
- <RxIrq>
Default depending on ETSEC type
- <NotUseDmaBuffers>
0 = FALSE | 1 = TRUE
- -fslfec <instance> <mode> <refboard> [--nopinmuxing] [--nomacaddr]
- Hardware: Freescale FEC/ENET
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- <RefBoard>
mars | sabrelite | sabresd | imx28evk | topaz | imxceetul2 | mimxrt1064-evk | imx93evk | custom
- If custom:
- <FecType>
imx25 | imx28 | imx53 | imx6 | vf6 | imx7 | imx8 | imx8m | imxrt1064 | imx9
- <PhyInterface>
fixed | mii | rmii | rmii50Mhz | gmii | sgmii | rgmii | osdriver
- <PhyAddress>
0 … 31, default 0 (don’t use if osdriver)
- Optional:
- --nopinmuxing
No pin muxing
- Optional:
- --nomacaddr
Don’t read MAC address
- -gem <instance> <mode> <refboard> [--osdriver] [--clkdivtype_k26] [--nopinmuxing]
- Hardware: Cadence GEM/MACB
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- <RefBoard>
zc702 | zedboard | microzed | zcu102 | zcu104 | KR260 | rpi5 | polarfire | custom
- If custom:
- <PhyAddress>
0 … 31
- <PhyConnectionMode>
MIO (0) or EMIO (1)
- <UseGmiiToRgmii>
Use Xilinx GmiiToRgmii converter TRUE (1) or FALSE (0)
- <GmiiToRgmiiPort>
GmiiToRgmii converter PHY address 0 … 31
- <GemType>
zynq7000 | ultrascale | bcm2712 | polarfire
- Optional:
- --osdriver
PhyInterface osdriver
- Optional:
- --clkdivtype_k26
Clock divisor
- Optional:
- --nopinmuxing
Don’t use pin muxing
- -intelgbe <instance> <mode> [--tts <sendoffset>|--tmr] [--nophyctrlonconnect]
- Hardware: Intel Pro/1000 network adapter card
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- Optional:
- --tts
Enable Real-time Ethernet Driver Time Triggered Send (TTS)
- <SendOffset>
TTS cyclic frame send offset from cycle start (usec)
- or
- --tmr
Enable Real-time Ethernet Driver Timer
- Optional:
- --nophyctrlonconnect
Disable PHY control (e.g. PHY reset, PHY PM settings, Gbits Ctrl) on link connection detected
- -i8255x <instance> <mode>
- Hardware: Intel Pro/100 network adapter card
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- -icss <instance> <mode> <masterflag> <refboard> [--mii <phyaddress>|--osdriver]
- \ [--nophyreset] [--tts <sendoffset>]
- Hardware: Texas Instruments Board with PRUSS
- <Instance>
ICSS Port (100 Mbit/s) 1 … 4
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- <MasterFlag>
(m) Master (Initialize board, mdio, both phy) or (s) Slave
- <RefBoard>
am572x-idk | am571x-idk | am3359-icev2 | am574x
- Optional:
- --mii
PhyInterface mii
- <PhyAddress>
0 … 31
- or
- --osdriver
PhyInterface osdriver
- Optional:
- --nophyreset
No PHY Reset
- Optional:
- --tts
Enables Real-time Ethernet Driver Time Triggered Send (TTS)
- <SendOffset>
TTS cyclic frame send offset from cycle start [us]
- -icssg <instance> <mode> <masterflag> <refboard>
- Hardware: Texas Instruments AARCH64 Board with Gigabit PRUSS
- <Instance>
ICSSG Port 1 … 6
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- <MasterFlag>
(m) Master (Initialize board, mdio, both phy) or (s) Slave
- <RefBoard>
am654x-idk
- -l9218i <instance> <mode>
- Hardware: SMSC LAN9218i/LAN9221
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- -lan743x <instance> <mode>
- Hardware: Microchip LAN743x
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
1 = Polling mode
- -ndis <ipaddress> <mode> [--name <adaptername>] [--disablepromiscuousmode]
- \ [--disableforcebroadcast]
- Hardware: Hardware independent, only available for Windows.
- <IpAddress>
IP address of network adapter card, e.g. 192.168.157.2 or 0.0.0.0 if name given
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- Optional:
- --name
Select network adapter by name
- <AdapterName>
Service name from HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows NT\CurrentVersion\NetworkCards
- Optional:
- --disablepromiscuousmode
Disable promiscuous mode
- Optional:
- --disableforcebroadcast
Disable force broadcast
- -multiplier <instance> <mode> [--type <type>] --port <port> --link <link parms>
- Hardware: Beckhoff CUxxxx Ethernet-Port-Multiplier
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode | 1 = Polling mode, for now only polling mode is supported
- --port
Multiplier port in use
- <Port>
0 = X1, 1 = X2, …
- --link
Link parameters of network adapter connected to the uplink port
- <Link parms>
e.g. -intelgbe …
- Optional:
- --type
Multiplier type
- <Type>
cu2508 = CU2508 Ethernet-Port-Multiplier | et2000 = ET2000 Multichannel Ethernet-Probe
- -remote <instance> <mode> <src ip> <src port> <dst ip> <dst port> [--mac <address>]
- \ [--rxbuffercnt <count>]
Hardware: Hardware independent. Tunnels EtherCAT frames through a TCP socket
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
1 = Polling mode
- <Src ip>
Source adapter IP address (listen)
- <Src port>
Source port number (listen)
- <Dst ip>
Destination adapter IP address (connect)
- <Dst port>
Destination port number (connect)
- Optional:
- --mac
MAC Address
- <Address>
formatted as xx:xx:xx:xx:xx:xx or xx-xx-xx-xx-xx-xx
- Optional:
- --rxbuffercnt
Frame buffer count for interrupt service thread (IST)
- <Count>
Buffer count
- -r6040 <instance> <mode>
- Hardware: RDC R6040
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
1 = Polling mode
- -rtl8139 <instance> <mode>
- Hardware: Realtek RTL8139
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- -rtl8169 <instance> <mode>
- Hardware: Realtek RTL8168 / RTL8169 / RTL8111
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- -sheth <instance> <mode> <refboard>
- Hardware: Renesas RZG1 or Armadillo-800 EVA or MYIR Remi Pi (Renesas RZ/G2L) or Renesas RX72N Envision Kit
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
1 = Polling mode
- <RefBoard>
rzg1e | a800eva | rzg2l | rx72n
- -snarf <adaptername>
- Hardware: Hardware independent, only available for VxWorks
- <AdapterName>
Adapter name, e.g. fei0
- -sockraw <device> [<mode>] [--nommaprx] [--promiscuousmode]
- Hardware: Hardware independent, only available for Linux.
- <Device>
Network adapter, e.g. eth1
- Optional:
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- Optional:
- --nommaprx
Disable PACKET_MMAP for receive
- Optional:
- --promiscuousmode
Enable promiscuous mode
- -sockxdp <device> <mode> [--queue <id>] [--xdpmode <mode>]
- Hardware: Hardware independent, only available for Linux.
- <Device>
Network adapter, e.g. eth1
- <Mode>
0 = Interrupt mode | 1 = Polling mode
- Optional:
- --queue
Set Queue Id
- <Id>
Queue Id, e.g. 0, 1, … (Default 0)
- Optional:
- --xdpmode
XDP Mode
- <Mode>
SKB(1), DRV(2), HW(3) or DRV_ZEROCOPY(4). Default is SKB(1)
- -stm32eth <instance> <mode>
- Hardware: STM32H7 Ethernet
- <Instance>
Device instance 1 = first, 2 = second, …
- <Mode>
1 = Polling mode
2.5. Compiling the EcMasterDemo
The following main rules can be used to generate the example applications for all operating systems.
<OS>is a placeholder for the operating system used.<ARCH>is a placeholder for the architecture. Different architectures are supported.
2.5.1. EtherCAT® MainDevice Software Development Kit (SDK)
The EtherCAT® MainDevice development kit is needed to write applications based on the MainDevice stack. The MainDevice stack is shipped as a library which is linked together with the application.
- The following components are supplied together with an SDK:
<InstallPath>/Bin <InstallPath>/Doc <InstallPath>/SDK <InstallPath>/SDK/INC <InstallPath>/SDK/LIB <InstallPath>/SDK/FILES <InstallPath>/Sources/Common
/BinExecutables containing the MainDevice stack
/DocDocumentation
/ExamplesOne or more example applications using a predefined EtherCAT® configuration. It is easily adaptable to different configurations using an appropriate EtherCAT® configuration XML file.
/SDKEtherCAT® Software Development Kit containing libraries and header files to build C/C++-applications
/SDK/INC:Header files to be included with the application
/SDK/LIB:Libraries to be linked with the application
/SDK/FILES:Additional files for platform integration (e.g. Windows CE registry files)
/Sources/Common:Shared .cpp-files
2.5.2. Include search path
- The header files are located in the following directories:
<InstallPath>/SDK/INC <InstallPath>/SDK/INC/<OS>/<ARCH> <InstallPath>/Sources/Common
2.5.3. Libraries
- The libraries are located in the following directories:
<InstallPath>/SDK/LIB/<OS>/<ARCH>