5.7. Beckhoff CCAT - emllCCAT
The parameters to the Real-time Ethernet Driver CCAT are setup-specific.
The function CreateLinkParmsFromCmdLineCCAT() in EcSelectLinkLayer.cpp demonstrates how to initialize the Real-time Ethernet Driver instance.
Because the link status cannot be read quickly from a register of the adapter, it will not be automatically refreshed like by the other Real-time Ethernet Drivers.
-
struct EC_T_LINK_PARMS_CCAT
Public Members
-
EC_T_LINK_PARMS linkParms
Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_CCAT.
-
EC_T_CCAT_TYPE eCcatType
CCAT connection type
-
EC_T_LINK_PARMS linkParms
5.7.1. Supported PCI devices
Beckhoff CCAT PCI specific definitions (VendorId, DeviceId)
|