5.10. Texas Instruments CPSWG for AM6x and Jacinto 7 - emllCPSWG
The parameters to the CPSWG Real-time Ethernet Driver are setup-specific.
The function CreateLinkParmsFromCmdLineCPSWG() in EcSelectLinkLayer.cpp demonstrates how to initialize the Real-time Ethernet Driver instance.
-
struct EC_T_LINK_PARMS_CPSWG
Public Members
-
EC_T_LINK_PARMS linkParms
Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_CPSWG.
-
EC_T_DWORD dwPhyAddr
PHY address
-
EC_T_PHYINTERFACE ePhyInterface
PHY interface type
-
EC_T_BOOL bMaster
EC_TRUE: Initialize MAC
-
EC_T_DWORD dwTxDmaDesCnt
Transmit DMA descriptor buffer count. Maximum 500.
-
EC_T_DWORD dwRxDmaDesCnt
Receive DMA descriptor buffer count. Maximum 500.
-
EC_T_BOOL bNotUseDmaBuffers
EC_FALSE: Use buffers from DMA for receive (default), EC_TRUE: use buffers from heap for receive. EcLinkAllocSendFrame is not supported if bNotUseDmaBuffers = EC_TRUE.
-
EC_T_LINK_PARMS linkParms
5.10.1. CPSWG usage under Linux
The unbind feature of the am65-cpsw-nuss Linux driver isn’t supported and the atemsys kernel module must be assigned as driver for the platform device.
So the "ethernet/am654-cpsw-nuss" device tree node must be modified, by changing compatible = "atemsys"; and adding atemsys-Ident = "CPSWG"; and atemsys-Instance = <0x1>;, also remove or comment out dma-coherent;.
ethernet@46000000 {
compatible = "atemsys";
atemsys-Ident = "CPSWG";
atemsys-Instance = <0x1>;
...
#dma-coherent;
...
So the "ethernet/am642-cpsw-nuss" device tree node must be modified likewise.
Second port of am642-cpsw-nuss is not supported.
ethernet@8000000 {
compatible = "atemsys";
atemsys-Ident = "CPSWG";
atemsys-Instance = <0x1>;
...
#dma-coherent;
...
Currently following Linux versions are supported:
ti-processor-sdk-linux-rt-am65xx-evm-07_01_00_18 (tested on AM65 IDK)
ti-processor-sdk-linux-rt-am65xx-evm-08.06.00.47 (tested on AM65 IDK)
ti-processor-sdk-linux-rt-j7-evm-08_06_01_02 (tested on SK-TDA4VM)
ti-processor-sdk-linux-rt-j7-evm-08_06_01_02 (tested on SK-TDA4VM)
ti-processor-sdk-linux-edgeai-j721e-evm-09_01_00_06 (tested on SK-TDA4VM)
ti-processor-sdk-linux-rt-am64xx-evm-08.02.00.14 (tested on TMDS64GPEVM)
ti-processor-sdk-linux-rt-am64xx-evm-09.02.00.08 (tested on TMDS64GPEVM)
SolidRun ti_am64x_build/20240221 microsd-debian-bookworm-sr1 (tested on AM64 HummingBoard-T)
toradex_ti-linux-6.1.y Linux/arm64 6.1.46 Kernel (tested on Toradex Verdin AM62)