5.31. Linux SockRaw - emllSockRaw
emllSockRaw is part of EC-Master for Linux. emllSockRaw uses the network interface of the native driver, e.g., eth0, eth1, etc. The network adapter must be exclusively used for EtherCAT® and cannot be used for LAN (local area network) at the same time. Because the native Linux driver for the network adapter type is typically not fully real-time capable, it cannot be used for real time applications. If possible, an acontis Real-time Ethernet Driver, e.g. emllIntelGbe, should be used instead. emllSockRaw does not need the atemsys driver.
Note
Root privileges are required. A cycle time of 4 ms or higher may be needed.
- To run the application without root privileges, set the Linux capability ‘cap_net_raw’ to the application.
$ sudo setcap 'cap_net_raw+pe' ./EcMasterDemo
- To run python scripts without root privileges, create a Python environment and set the Linux capability ‘cap_net_raw’ to the python interpreter.
$ cd Bin/Linux $ python3 -m venv --copies PyEnv/ $ source PyEnv/bin/activate $ sudo setcap 'cap_net_raw+pe' PyEnv/bin/python3
The parameters to emllSockRaw are setup-specific. The function CreateLinkParmsFromCmdLineSockRaw() in EcSelectLinkLayer.cpp demonstrates how to initialize the parameters.
-
struct EC_T_LINK_PARMS_SOCKRAW
Public Members
-
EC_T_LINK_PARMS linkParms
Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_SOCKRAW.
-
EC_T_CHAR szAdapterName[EC_SOCKRAW_ADAPTER_NAME_SIZE]
Native ETH device name, e.g. “eth0” (zero terminated)
-
EC_T_BOOL bDisableForceBroadcast
Don’t change target MAC address to FF:FF:FF:FF:FF:FF
-
EC_T_BOOL bReplacePaddingWithNopCmd
Prevent adding Ethernet padding to work-around EtherCAT corruption bugs from native Linux driver(s)
-
EC_T_BOOL bUsePacketMmapRx
Use PACKET_MMAP PACKET_RX_RING for receive
-
EC_T_BOOL bSetCoalescingParms
Set Coalescing parameters to enhance the link layer performance
-
EC_T_BOOL bSetPromiscuousMode
Enable promiscuous mode at network adapter
-
EC_T_LINK_PARMS linkParms