Application programming interface, reference

9. Application programming interface, reference

Function prototypes, definitions etc. of the API can be found in the header file EcMonitor.h which is the main header file to include when using EC-Monitor.

Fundamental types

typedef void *EC_T_PVOID

Pointer of type void

typedef int EC_T_BOOL

Boolean

typedef char EC_T_CHAR

Character, 8 bit

typedef unsigned short EC_T_WCHAR

Wide-character, 16 bit

typedef unsigned char EC_T_BYTE

Byte, unsigned integer 8 bit

typedef unsigned char *EC_T_PBYTE

Pointer of type EC_T_BYTE

typedef unsigned short EC_T_WORD

Word, unsigned integer 16 bit

typedef unsigned int EC_T_DWORD

Double word, unsigned integer 32 bit

typedef signed char EC_T_SBYTE

Signed-Byte, signed integer 8 bit

typedef signed short EC_T_SWORD

Signed-Word, signed integer 16 bit

typedef signed int EC_T_SDWORD

Signed-Double-Word, signed integer 32 bit

typedef int EC_T_INT

Integer

typedef unsigned int EC_T_UINT

Unsigned-Integer

typedef short EC_T_SHORT

Short

typedef unsigned short EC_T_USHORT

Unsigned-Short

typedef float EC_T_REAL

Real, floating point

typedef double EC_T_LREAL

long Real, floating point

typedef unsigned long long EC_T_UINT64

Unsigned integer 64 bits

typedef signed long long EC_T_INT64

Signed integer 64 bits

EC_T_VOID

Void type

Macros

EC_TRUE

Boolean value: True

EC_FALSE

Boolean value: False

EC_NULL

Null pointer constant