10.1. Notification callback
-
typedef EC_T_DWORD (*EC_PF_NOTIFY)(EC_T_DWORD dwCode, EC_T_NOTIFYPARMS *pParms)
-
struct EC_T_NOTIFYPARMS
Data structure filled with detailed information about the according notification.
Public Members
-
EC_T_VOID *pCallerData
[in] Client depending caller data parameter. This pointer is one of the parameters when the client registers.
-
EC_T_BYTE *pbyInBuf
[in] Notification input parameters
-
EC_T_DWORD dwInBufSize
[in] Size of notification input parameters in bytes
-
EC_T_BYTE *pbyOutBuf
[out] Buffer for notification output (result)
-
EC_T_DWORD dwOutBufSize
[in] Size of buffer at pbyOutBuf in bytes
-
EC_T_DWORD *pdwNumOutData
[out] Amount of bytes written to pbyOutBuf by notification. EC_NULL: amount not set by notification.
-
EC_T_VOID *pCallerData