3. Ethernet TAP

To capture the EtherCAT® traffic, EC-Monitor supports a variety of different Ethernet Test Access Points (TAP). These can be special real-time optimized TAPs with minimal propagation delay and extended diagnostic options, or simple 100MBit/s Ethernet switches. The only requirement is that the input (RX) and output (TX) traffic is forwarded to the EC-Monitor via a common up-link port.

The various Ethernet TAP devices can be automatically detected by the EC-Monitor via EC_T_MONITOR_INIT_PARMS::eEthTapType set to EC_T_ETHERNET_TAP_TYPE::eEthTap_AutoDetect.

3.1. TAP positioning

The Ethernet TAP device should be inserted in the network between the EtherCAT® MainDevice and SubDevices or, if this is not possible, between two SubDevices. The position of the Ethernet TAP is detected automatically and the EtherCAT® traffic is processed accordingly.

Diagram showing the recommended TAP placement between the EtherCAT MainDevice and SubDevices for traffic monitoring

For configurations where the EtherCAT® MainDevice has a direct interface to the SubDevices without an RJ45 cable, e.g. Beckhoff IPCs it is possible to connect the input port of the Ethernet TAP device to the RJ45 port of the topologically last SubDevice. The output port of the Ethernet TAP device must be bridged using an RJ45 loopback plug so that the EtherCAT® frames are forwarded back to the MainDevice.

Diagram showing an alternative TAP placement with the TAP connected to the last SubDevice RJ45 port and a loopback plug on the output to return frames to the MainDevice

In configurations where the TAP can only be inserted at an EtherCAT® Junction SubDevice, the port closest to the end of the topology should be used. Any SubDevices connected to the subsequent port will no longer be detected.

Diagram showing a TAP inserted at an EtherCAT Junction SubDevice using the port closest to the end of the topology, with a warning that SubDevices on subsequent ports will not be detected

Warning

Positioning the TAP within the topology can lead to inconsistencies in the process data image. This affects the outputs of the SubDevices preceding the TAP and that are read by a Logical Read-Write (LRW) command. The affected outputs are set to 0 by the EC-Monitor.

3.2. Generic 100MBit/s Ethernet Switch

A generic 100MBit/s Ethernet switch with at least 3 ports can be used with EC-Monitor. The propagation delay can be up to several hundred μs per port and should therefore only be used for slower cycle times.

To manually select this device set EC_T_MONITOR_INIT_PARMS::eEthTapType to EC_T_ETHERNET_TAP_TYPE::eEthTap_Generic.

3.3. Beckhoff ET2000

The Beckhoff ET2000 comes with propagation delay below 1 μs, a high-precision timestamp and extended frame error detection capabilities. The TAP offers the possibility to determine on which port the frame was received. The EC-Monitor uses this to evaluate whether it is a TX or RX frame. Therefore, the outgoing connection from the EtherCAT® MainDevice should be connected to either port X1.0, X2.0, X3.0 or X4.0.

To manually select this device set EC_T_MONITOR_INIT_PARMS::eEthTapType to EC_T_ETHERNET_TAP_TYPE::eEthTap_Beckhoff_ET2000.

To filter frames by line, set EC_T_MONITOR_INIT_PARMS::wMainTapPortIn and EC_T_MONITOR_INIT_PARMS::wMainTapPortOut accordingly.

3.4. Dualcomm ETAP-1000

The Dualcomm ETAP-1000 has a propagation delay below 1 μs. Since it has no other extended capabilities it can be used as generic Ethernet TAP EC_T_ETHERNET_TAP_TYPE::eEthTap_Generic.

3.5. Kunbus TAP Curious

The Kunbus TAP Curious comes with propagation delay below 1 μs, a high-precision timestamp and extended frame error detection capabilities. The TAP offers the possibility to determine on which port the frame was received. The EC-Monitor uses this to evaluate whether it is a TX or RX frame. Therefore, the outgoing connection from the EtherCAT® MainDevice should be connected to either port A or C.

To manually select this device set EC_T_MONITOR_INIT_PARMS::eEthTapType to EC_T_ETHERNET_TAP_TYPE::eEthTap_Kunbus_TapCurious.

To filter frames by line, set EC_T_MONITOR_INIT_PARMS::wMainTapPortIn and EC_T_MONITOR_INIT_PARMS::wMainTapPortOut accordingly.

3.6. ProfiTap ProfiShark

The ProfiTap ProfiShark devices are USB3.0 based Ethernet TAPs with a propagation delay below 1 μs. To use it with EC-Monitor, the Hardware Timestamping feature must be disabled in the Featues Tab of ProfiShark Manager.

As the device appear as a virtual Ethernet interface in the operating system, it can be used as a generic Ethernet TAP EC_T_ETHERNET_TAP_TYPE::eEthTap_Generic.

3.7. Port Mirror

A TAP or switch with port mirroring functionality can also be used with EC-Monitor. Typically, a port mirroring device has four Ethernet ports, two input ports for the network and two mirroring output ports. Incoming traffic on the respective network port is mirrored to the corresponding mirror port.

In the EtherCAT® use case, this means that the Ethernet frames outgoing from the EtherCAT® MainDevice are mirrored on one port and the Ethernet frames returning from the EtherCAT® SubDevices are output on another port. Since EC-Monitor currently only supports one port for connecting to the TAP, the mirror port with the returning Ethernet frames must be connected.

Diagram of a port mirror TAP configuration where the mirror port receiving returning EtherCAT frames is connected to the EC-Monitor uplink

This network adapter must be selected manually by setting EC_T_MONITOR_INIT_PARMS::eEthTapType to EC_T_ETHERNET_TAP_TYPE::eEthTap_PortMirror.

Warning

Since only the returning frames are processed, inconsistencies occur in the process data image of the outputs for EtherCAT® frames with LRW commands.