6.1. Example application

The example application will handle the following tasks:

  • EC-Monitor initialization

  • Process Data acquisition with EC-Daq

  • Periodic Job Task in polling or interrupt mode

  • Thread with periodic tasks and application thread already implemented

  • Record and replay wireshark traces

  • Logging. The output messages of the demo application will be printed on the console as well as in some files

  • “Out of the box” solution for different operating systems: Windows, Linux …

6.1.1. File reference

The EcMonitorDemo application consists of the following files:

File reference diagram showing the source files of the EcMonitorDemo application including EcDemoMain, EcDemoApp, EcNotification, and supporting modules

Filename

Description

EcDemoMain.cpp

Entry point for the different operating systems

EcDemoPlatform.h

Operating system specific settings (task priorities, timer settings)

EcDemoApp.cpp

Initialize, start and terminate EC-Monitor

EcDemoApp.h

Application specific settings for EcDemoApp

EcDemoParms.cpp

Parsing of command line parameters

EcDemoParms.h

Basic configuration parameters

EcSelectLinkLayer.cpp

Common Functions which abstract the command line parsing into Real-time Ethernet Driver parameter

EcNotification.cpp

SubDevice monitoring and error detection (function ecatNotify() )

EcSlaveInfo.cpp

SubDevice information services

EcLogging.cpp

Message logging functions

EcTimer.cpp

Start and monitor timeouts

6.1.2. EC-Monitor life cycle

Basically the operation of the EC-Monitor is wrapped between the functions

and

The EC-Monitor is made ready for operation and started with the first two functions mentioned. During this preparation, a thread is set up and started that handles all the cyclic tasks of the EC-Monitor. The last function stops the EC-Monitor and clears the memory.

An overview of the complete life cycle as a sequence diagram:

skinparam monochrome true
skinparam SequenceMessageAlign direction
hide footbox

participant EcDemoMain
participant EcDemoApp
participant EcEmbedded as "EC-Monitor"
participant JobTask as "EcMonitorJobTask"
participant EcTimingTask

activate EcDemoMain
EcDemoMain->EcDemoMain : PrepareCommandLine()
EcDemoMain->EcDemoMain : SetAppParmsFromCommandLine()
EcDemoMain->EcDemoMain : InitLogging()
EcDemoMain->EcTimingTask : CreateTimingTask(pvJobTaskEvent)
activate EcTimingTask
EcDemoMain->EcDemoApp : EcDemoApp()

activate EcDemoApp
EcDemoApp->EcDemoApp : InitNotificationHandler()
EcDemoApp->EcEmbedded : emonInitMonitor()
activate EcEmbedded
EcDemoApp<--EcEmbedded
EcDemoApp->EcEmbedded : emonConfigureNetwork()
EcDemoApp<--EcEmbedded

EcDemoApp->JobTask : CreateJobTask()
activate JobTask

par
    loop
        EcTimingTask->EcTimingTask : sleep()
        EcTimingTask->JobTask : OsSetEvent(pvJobTaskEvent)
        activate JobTask
    end
else
    JobTask->EcEmbedded : emonExecJob(ProcessAllRxFrames)
    JobTask<--EcEmbedded
    JobTask->JobTask : myAppWorkPd()
    JobTask->EcEmbedded : emonExecJob(MonitorTimer)
    JobTask<--EcEmbedded
    deactivate JobTask
else
    EcDemoApp->EcEmbedded : emonRasSrvStart()
    EcDemoApp<--EcEmbedded
    EcDemoApp->EcEmbedded : emonRegisterClient()
    EcDemoApp<--EcEmbedded
    EcDemoApp->EcDemoApp : idle()
    EcDemoApp->JobTask : shutdownJobTask()
    deactivate JobTask
end

EcDemoApp->EcEmbedded : emonUnregisterClient()
EcDemoApp<--EcEmbedded
EcDemoApp->EcEmbedded : emonRasSrvStop()
EcDemoApp<--EcEmbedded
EcDemoApp->EcEmbedded : emonDeinitMonitor()
EcDemoApp<--EcEmbedded
deactivate EcEmbedded

EcDemoMain<--EcDemoApp
deactivate EcDemoApp
EcDemoMain->EcTimingTask : shutdownTimingTask()
deactivate EcTimingTask
EcDemoMain->EcDemoMain : DeinitLogging()

A more detailed description of the functions:

EcDemoMain()

A wrapper to start the demo from the respective operating system. In addition to initializing the operating system, parsing command line parameters and initializing logging it also starts the timing task.

EcDemoApp()

Demo application. The function takes care of starting and stopping the EC-Monitor and all related tasks. In between, the function runs idle, while all relevant work is done by the EcMonitorJobTask().

EcMonitorJobTask()

Thread that does the necessary periodic work. Very important here is myAppWorkPd() between eUsrJob_ProcessAllRxFrames and eUsrJob_MonitorTimer. Application-specific access to the process data image can be made here, which is synchronous with the bus cycle.

EcTimingTask()

Timing Thread. This thread sets the timing event that triggers the EcMonitorJobTask for the next cycle.

emonInitMonitor()

Prepare the EC-Monitor for operation and set operational parameters, e.g. used Real-time Ethernet Driver, buffer sizes, maximum number of SubDevices, … .

emonConfigureNetwork()

Loads the configuration from the ENI (XML file).

emonRegisterClient()

Register the application as a client at the EC-Monitor to receive event notifications.

emonDeinitMonitor()

Clean up.