9.9. File access over EtherCAT® (FoE)

The EC-Monitor can record file transfers via the FoE protocol between an EtherCAT® MainDevice and a SubDevice. These FoE transfers can be forwarded to the application as segmented packets in real time via the notifications emonNotify - eMbxTferType_FOE_SEG_DOWNLOAD and emonNotify - eMbxTferType_FOE_SEG_UPLOAD.

In addition, the FoE transfers can be stored as a file on the file system. The files are automatically created and stored in EC_T_MONITOR_INIT_PARMS::szFileStoragePath. The file name consists of the following:
<TimeStamp[msec]>_Slave<StationAddress>_<FoeFileName>
For example:
0123456789_Slave1001_firmware.bin

The notifications for FoE can be deactivated using the EC_T_MBX_PARMS_FOE::bDisableNotifications parameter if they are not required or to save computing time. If no file system is available or file storage is not desired, it can be disabled using the EC_T_MBX_PARMS_FOE::bDisableFileStorage parameter.

If both parameters EC_T_MBX_PARMS_FOE::bDisableNotifications and EC_T_MBX_PARMS_FOE::bDisableFileStorage are set, the FoE monitoring is completely deactivated.

9.9.1. Notification sequence

Once the EC-Monitor detects an FoE transfer, the application is notified via an emonNotify - eMbxTferType_FOE_DOWNLOAD_REQ or emonNotify - eMbxTferType_FOE_UPLOAD_REQ notification. This notification contains basic information about the upcoming transfer, e.g. requested file name.

After that, each individual packet is transmitted via an emonNotify - eMbxTferType_FOE_SEG_DOWNLOAD or emonNotify - eMbxTferType_FOE_SEG_UPLOAD notification. The end of the transfer is set via the EC_T_MBXTFER::eTferStatus = eMbxTferStatus_TferDone.

Download

skinparam monochrome true
skinparam SequenceMessageAlign direction
skinparam SequenceBoxBorderColor transparent
skinparam ParticipantPadding 50
hide footbox

participant MainDevice
participant Monitor
participant SubDevice
participant App

MainDevice->SubDevice: WRQ(file name)
activate Monitor
Monitor->App: eMbxTferType_FOE_DOWNLOAD_REQ\neMbxTferStatus_Pend
deactivate Monitor

MainDevice->SubDevice: DATA(first packet)
activate Monitor
Monitor->App: eMbxTferType_FOE_SEG_DOWNLOAD\neMbxTferStatus_Pend
deactivate Monitor

...
MainDevice->SubDevice: DATA(last packet)
activate Monitor
Monitor->App: eMbxTferType_FOE_SEG_DOWNLOAD\neMbxTferStatus_Done
deactivate Monitor

Upload

skinparam monochrome true
skinparam SequenceBoxBorderColor transparent
skinparam ParticipantPadding 50
hide footbox

participant MainDevice
participant Monitor
participant SubDevice
participant App

MainDevice->SubDevice: RRQ(file name)
activate Monitor
Monitor->App: eMbxTferType_FOE_UPLOAD_REQ\neMbxTferStatus_Pend
deactivate Monitor

SubDevice->MainDevice: DATA(first packet)
activate Monitor
Monitor->App: eMbxTferType_FOE_SEG_UPLOAD\neMbxTferStatus_Pend
deactivate Monitor

...
SubDevice->MainDevice: DATA(last packet)
activate Monitor
Monitor->App: eMbxTferType_FOE_SEG_UPLOAD\neMbxTferStatus_Done
deactivate Monitor

9.9.2. emonNotify - eMbxTferType_FOE_DOWNLOAD_REQ

Notifies an FoE download request from the EtherCAT® MainDevice to a SubDevice.

emonNotify - eMbxTferType_FOE_DOWNLOAD_REQ
Parameter
  • pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, containing the corresponding mailbox transfer object

  • dwInBufSize: [in] Size of the transfer object pbyInBuf in bytes

  • pbyOutBuf: [out] Should be set to EC_NULL

  • dwOutBufSize: [in] Should be set to 0

  • pdwNumOutData: [out] Should be set to EC_NULL

The parameters that the MainDevice has requested from the SubDevice are stored in the structure EC_T_MBX_DATA::FoE_Request which is part of EC_T_MBXTFER::MbxData.

struct EC_T_MBX_DATA_FOE_REQ

Public Members

EC_T_WORD wStationAddress

[out] Station address of the slave

EC_T_DWORD dwPassword

[out] FoE read/write request password

EC_T_CHAR szFileName[EC_MAX_FILE_NAME_SIZE]

[out] Name of the file to be read/write

9.9.3. emonNotify - eMbxTferType_FOE_SEG_DOWNLOAD

Transmits a data segment of the ongoing FoE download.

emonNotify - eMbxTferType_FOE_SEG_DOWNLOAD
Parameter
  • pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, containing the corresponding mailbox transfer object

  • dwInBufSize: [in] Size of the transfer object pbyInBuf in bytes

  • pbyOutBuf: [out] Should be set to EC_NULL

  • dwOutBufSize: [in] Should be set to 0

  • pdwNumOutData: [out] Should be set to EC_NULL

The FoE download data segment is stored at EC_T_MBXTFER::pbyMbxTferData with size EC_T_MBXTFER::dwDataLen and may have to be buffered by the application. Access to the memory area EC_T_MBXTFER::pbyMbxTferData outside of the notification caller context is illegal and the results are undefined.

Information about the current transfer is stored in the structure EC_T_MBX_DATA::FoE which is part of EC_T_MBXTFER::MbxData. Among other things, it contains the SubDevice station address EC_T_MBX_DATA_FOE::wStationAddress and the number of bytes already transmitted EC_T_MBX_DATA_FOE::dwTransferredBytes.

struct EC_T_MBX_DATA_FOE

Public Members

EC_T_DWORD dwTransferredBytes

[out] Amount of transferred bytes

EC_T_DWORD dwRequestedBytes

[out] Amount of bytes to be provided by the application

EC_T_DWORD dwBusyDone

[out] If slave is busy: 0 … dwBusyEntire

EC_T_DWORD dwBusyEntire

[out] If dwBusyEntire > 0: Slave is busy

EC_T_CHAR szBusyComment[EC_FOE_BUSY_COMMENT_SIZE]

[out] Busy Comment from slave

EC_T_DWORD dwFileSize

[out] File size

EC_T_WORD wStationAddress

[out] Station address of the slave

Note

The elements EC_T_MBX_DATA_FOE::dwRequestedBytes and EC_T_MBX_DATA_FOE::dwFileSize are not used by the EC-Monitor because they are not known at runtime.

9.9.4. emonNotify - eMbxTferType_FOE_UPLOAD_REQ

Notifies an FoE upload request from the EtherCAT® MainDevice to a SubDevice.

emonNotify - eMbxTferType_FOE_DOWNLOAD_REQ
Parameter
  • pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, containing the corresponding mailbox transfer object

  • dwInBufSize: [in] Size of the transfer object pbyInBuf in bytes

  • pbyOutBuf: [out] Should be set to EC_NULL

  • dwOutBufSize: [in] Should be set to 0

  • pdwNumOutData: [out] Should be set to EC_NULL

The parameters that the MainDevice has requested from the SubDevice are stored in the structure EC_T_MBX_DATA::FoE_Request which is part of EC_T_MBXTFER::MbxData.

struct EC_T_MBX_DATA_FOE_REQ
EC_T_WORD wStationAddress
EC_T_DWORD dwPassword
EC_T_CHAR szFileName[EC_MAX_FILE_NAME_SIZE]

9.9.5. emonNotify - eMbxTferType_FOE_SEG_UPLOAD

Transmits a data segment of the ongoing FoE upload.

emonNotify - eMbxTferType_FOE_SEG_UPLOAD
Parameter
  • pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, containing the corresponding mailbox transfer object

  • dwInBufSize: [in] Size of the transfer object pbyInBuf in bytes

  • pbyOutBuf: [out] Should be set to EC_NULL

  • dwOutBufSize: [in] Should be set to 0

  • pdwNumOutData: [out] Should be set to EC_NULL

The FoE upload data segment is stored at EC_T_MBXTFER::pbyMbxTferData with size EC_T_MBXTFER::dwDataLen and may have to be buffered by the application. Access to the memory area EC_T_MBXTFER::pbyMbxTferData outside of the notification caller context is illegal and the results are undefined.

Information about the current transfer is stored in the structure EC_T_MBX_DATA::FoE which is part of EC_T_MBXTFER::MbxData. Among other things, it contains the SubDevice station address EC_T_MBX_DATA_FOE::wStationAddress and the number of bytes already transmitted EC_T_MBX_DATA_FOE::dwTransferredBytes.

struct EC_T_MBX_DATA_FOE
EC_T_DWORD dwTransferredBytes
EC_T_DWORD dwRequestedBytes
EC_T_DWORD dwBusyDone
EC_T_DWORD dwBusyEntire
EC_T_CHAR szBusyComment[EC_FOE_BUSY_COMMENT_SIZE]
EC_T_DWORD dwFileSize
EC_T_WORD wStationAddress

Note

The elements EC_T_MBX_DATA_FOE::dwRequestedBytes and EC_T_MBX_DATA_FOE::dwFileSize are not used by the EC-Monitor because they are not known at runtime.

9.9.6. emonNotify - EC_NOTIFY_FOE_MBSLAVE_ERROR

This error will be indicated in case an FoE mailbox SubDevice sends an error message. Detailed error information is stored in the structure EC_T_MBOX_FOE_ABORT_DESC which is part of EC_T_ERROR_NOTIFICATION_DESC.

struct EC_T_MBOX_FOE_ABORT_DESC

Public Members

EC_T_SLAVE_PROP SlaveProp

Slave properties

EC_T_DWORD dwErrorCode

Error code

EC_T_CHAR achErrorString[MAX_STD_STRLEN]

FoE error string

9.9.7. emonConvertEcErrorToFoeError

EC_T_DWORD emonConvertEcErrorToFoeError(EC_T_DWORD dwInstanceID, EC_T_DWORD dwErrorCode)

Convert master error code to FoE error code.

Returns:

FoE error code according to ETG1000.6 Table 92 - Error codes of FoE