9.6. Real-time Ethernet Driver Control Interface

9.6.2. emonIoCtl - EC_IOCTL_GET_LINKLAYER_MODE

EC_IOCTL_GET_LINKLAYER_MODE

Get Real-time Ethernet Driver mode (EcLinkMode_POLLING, EcLinkMode_INTERRUPT)

Parameters:
  • pbyInBuf – [in] Should be set to EC_NULL

  • dwInBufSize – [in] Should be set to 0

  • pbyOutBuf – [out] Pointer to struct EC_T_LINKLAYER_MODE_DESC

  • dwOutBufSize – [in] Size of the output buffer in bytes

  • pdwNumOutData – [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer.

Returns:

EC_E_NOERROR or error code

struct EC_T_LINKLAYER_MODE_DESC

Public Members

EC_T_LINKMODE eLinkMode

[out] Operation mode of main interface

EC_T_LINKMODE eLinkModeRed

[out] Operation mode of redundancy interface

See also

emonIoCtl()

9.6.3. emonIoCtl - EC_LINKIOCTL…

The generic control interface provides access to the main network adapter when adding EC_IOCTL_LINKLAYER_MAIN to the EC_LINKIOCTL parameter at dwCode.

EC_T_DWORD dwCode = (EC_IOCTL_LINKLAYER_MAIN | EC_LINKIOCTL_GET_ETHERNET_ADDRESS);

9.6.4. emonIoCtl - EC_LINKIOCTL_GET_ETHERNET_ADDRESS

Provides MAC addresses of main or red line.

emonIoCtl - EC_LINKIOCTL_GET_ETHERNET_ADDRESS
Parameter
  • pbyInBuf: [in] Should be set to EC_NULL

  • dwInBufSize: [in] Should be set to 0

  • pbyOutBuf: [out] Pointer to MAC address buffer (6 bytes)

  • dwOutBufSize: [in] Size of the output buffer in bytes (at least 6)

  • pdwNumOutData: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer.

See also

emonIoCtl()

9.6.5. emonIoCtl - EC_LINKIOCTL_GET_SPEED

emonIoCtl - EC_LINKIOCTL_GET_SPEED
Parameter
  • pbyInBuf: [in] Should be set to EC_NULL

  • dwInBufSize: [in] Should be set to 0

  • pbyOutBuf: [out] Pointer to EC_T_DWORD. Set by Real-time Ethernet Driver to 10/100/1000.

  • dwOutBufSize: [in] Size of the output buffer in bytes

  • pdwNumOutData: [out] Pointer to EC_T_DWORD. Amount of bytes written to the output buffer.

See also

emonIoCtl()