11.2. Application programming interface
11.2.1. emonRasSrvStart
-
EC_T_DWORD EC_NAMESPACE::emonRasSrvStart(const EC_T_RAS_SERVER_PARMS *pParms, EC_T_PVOID *ppHandle)
Starts the RAS Server.
- Parameters:
pParms – [in] Server start-up parameters
ppHandle – [out] Handle to opened instance, used for ctrl access
- Returns:
EC_E_NOERROR or error code
-
struct EC_T_RAS_SERVER_PARMS
Public Members
-
EC_T_DWORD dwSignature
[in] Set to EC_RAS_SERVER_SIGNATURE
-
EC_T_DWORD dwSize
[in] Set to sizeof(EC_T_RAS_SERVER_PARMS)
-
EC_T_LOG_PARMS LogParms
[in] Logging parameters
-
EC_T_IPADDR oAddr
[in] Remote Access Server (RAS) listen IP address
-
EC_T_WORD wPort
[in] Remote Access Server (RAS) listen port
-
EC_T_WORD wMaxClientCnt
[in] Max. clients in parallel (0: unlimited)
-
EC_T_DWORD dwCycleTime
[in] Cycle Time of RAS Network access (acceptor, worker)
-
EC_T_DWORD dwCommunicationTimeout
[in] Timeout [ms] before automatically closing connection
-
EC_T_DWORD dwAcceptorThreadPrio
[in] Acceptor Thread Priority
-
EC_T_DWORD dwAcceptorThreadStackSize
[in] Acceptor Thread Stack Size
-
EC_T_DWORD dwClientWorkerThreadPrio
[in] Client Worker Thread Priority
-
EC_T_DWORD dwClientWorkerThreadStackSize
[in] Client Worker Thread Stack Size
-
EC_T_DWORD dwMaxQueuedNotificationCnt
[in] Amount of concurrently queue able Notifications
-
EC_T_DWORD dwMaxParallelMbxTferCnt
[in] Amount of concurrent active mailbox transfers
-
EC_PF_NOTIFY pfnRasNotify
[in] Function pointer called to notify error and status information generated by Remote API Layer
-
EC_T_DWORD dwCycErrInterval
[in] Interval which allows cyclic Notifications
-
EC_T_DWORD dwMaxQueuedNotificationSize
[in] Size of concurrent active mailbox transfers
-
EC_T_BYTE *pbyTlsCert
[in] TLS certificate filename string
-
EC_T_DWORD dwTlsCertSize
[in] Size of TLS certeficate
-
EC_T_BYTE *pbyTlsPrivKey
[in] TLS private key filename string
-
EC_T_DWORD dwTlsPrivKeySize
[in] Size of TLS private key
-
EC_T_DWORD dwSignature
-
union EC_T_IPADDR
- #include <EthernetServices.h>
Public Members
-
EC_T_INNER_IPADDR sAddr
IPv4 address (endianness independent)
-
EC_T_DWORD dwAddr
Reserved, use EC_T_IPADDR::sAddr.by instead. OS-Layer socket API calls (SOCKADDR_IN::sin_addr).
-
EC_T_INNER_IPADDR sAddr
-
struct EC_T_INNER_IPADDR
Public Members
-
EC_T_BYTE by[4]
IPv4 address (endianness independent)
-
EC_T_BYTE by[4]
11.2.2. emonRasSrvStop
-
EC_T_DWORD EC_NAMESPACE::emonRasSrvStop(EC_T_PVOID pvHandle, EC_T_DWORD dwTimeout)
Stops the RAS Server.
- Parameters:
pvHandle – [in] Handle to previously started Server
dwTimeout – [in] Timeout [ms] used to shut down all spawned threads, it’s multiplied internally by the amount of threads spawned
- Returns:
EC_E_NOERROR or error code
11.2.3. emonRasNotify
Callback function called by Remote API Server in case of State changes or error situations.
-
typedef EC_T_DWORD (*EC_PF_NOTIFY)(EC_T_DWORD dwCode, EC_T_NOTIFYPARMS *pParms)
11.2.4. emonRasNotify - EC_RAS_NOTIFY_CONNECTION
Notification about a change in the Remote API’s state.
- emonRasNotify - EC_T_RAS_CONNOTIFYDESC
- Parameter
pbyInBuf: [in] Pointer to data of type EC_T_RAS_CONNOTIFYDESCdwInBufSize: [in] Size of the input buffer in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
-
struct EC_T_RAS_CONNOTIFYDESC
Public Members
-
EC_T_DWORD dwCause
[in] Cause of state connection state change
-
EC_T_DWORD dwCookie
[in] Unique identification cookie of connection instance
-
EC_T_DWORD dwCause
11.2.5. emonRasNotify - EC_RAS_NOTIFY_REGISTER
Notification that a connected application registered a client to the EC-Monitor.
- emonRasNotify - EC_RAS_NOTIFY_REGISTER
- Parameter
pbyInBuf: [in] Pointer to data of type EC_T_RAS_REGNOTIFYDESCdwInBufSize: [in] Size of the input buffer in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
-
struct EC_T_RAS_REGNOTIFYDESC
Public Members
-
EC_T_DWORD dwCookie
[in] Unique identification cookie of connection instance
-
EC_T_DWORD dwResult
[in] Result of registration request
-
EC_T_DWORD dwInstanceId
[in] Master Instance client registered to
-
EC_T_DWORD dwClientId
[in] Client ID of registered client
-
EC_T_DWORD dwCookie
11.2.6. emonRasNotify - EC_RAS_NOTIFY_UNREGISTER
Notification that a connected application un-registered a client from the EC-Monitor.
- emonRasNotify - EC_RAS_NOTIFY_UNREGISTER
- Parameter
pbyInBuf: [in] Pointer to data of type EC_T_RAS_REGNOTIFYDESCdwInBufSize: [in] Size of the input buffer in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
See also
11.2.7. emonRasNotify - EC_RAS_NOTIFY_MARSHALERROR
Notification about an error during marshalling in Remote API Server connection layer.
- emonRasNotify - EC_RAS_NOTIFY_MARSHALERRORDESC
- Parameter
pbyInBuf: [in] Pointer to data of type EC_T_RAS_MARSHALERRORDESCdwInBufSize: [in] Size of the input buffer in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
-
struct EC_T_RAS_MARSHALERRORDESC
Public Members
-
EC_T_DWORD dwCookie
[in] Unique identification cookie of connection instance
-
EC_T_DWORD dwCause
[in] Cause of the command marshalling error
-
EC_T_DWORD dwLenStatCmd
[in] Length of the faulty command
-
EC_T_DWORD dwCommandCode
[in] Command code of the faulty command
-
EC_T_DWORD dwCookie
11.2.8. emonRasNotify - EC_RAS_NOTIFY_ACKERROR
Notification about an error during creation of ack / nack packet.
- emonRasNotify - EC_RAS_NOTIFY_ACKERROR
- Parameter
pbyInBuf: [in] Pointer to EC_T_DWORD containing error codedwInBufSize: [in] Size of the input buffer in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
11.2.9. emonRasNotify - EC_RAS_NOTIFY_NONOTIFYMEMORY
Notification given, when no empty buffers for notifications are available in the pre-allocated notification store. This points to a configuration error.
- emonRasNotify - EC_RAS_NOTIFY_NONOTIFYMEMORY
- Parameter
pbyInBuf: [in] Pointer to EC_T_DWORD containing unique identification cookie of connection instancedwInBufSize: [in] Size of the input buffer in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
11.2.10. emonRasNotify - EC_RAS_NOTIFY_STDNOTIFYMEMORYSMALL
Notification given when the buffer size for standard notifications available in pre-allocated notification store is too small to carry a specific notification. This points to a configuration error.
- emonRasNotify - EC_RAS_NOTIFY_STDNOTIFYMEMORYSMALL
- Parameter
pbyInBuf: [in] Pointer to EC_T_DWORD containing unique identification cookie of connection instancedwInBufSize: [in] Size of the input buffer in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
11.2.11. emonRasNotify - EC_RAS_NOTIFY_MBXNOTIFYMEMORYSMALL
Notification given when the buffer size for Mailbox notifications available in pre-allocated notification store is too small to carry a specific notification. This points to a configuration error.
This is a serious error. If this error is given, Mailbox Transfer objects may have become out of sync and therefore no longer valid. Mailbox notifications should be dimensioned correctly, see emonRasSrvStart()
- emonRasNotify - EC_RAS_NOTIFY_MBXNOTIFYMEMORYSMALL
- Parameter
pbyInBuf: [in] Pointer to EC_T_DWORD containing unique identification cookie of connection instancedwInBufSize: [in] Size of the input buffer in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL