9.7. EtherCAT® Mailbox Transfer
To be able to initiate a mailbox transfer the client has to create a mailbox transfer object first.
This mailbox transfer object also contains the memory where the data to be transferred is stored.
The one client that initiated the mailbox transfer will be notified about a mailbox transfer completion by the emonNotify() callback function.
To be able to identify the transfer which was completed the client has to assign a unique transfer identifier for each mailbox transfer. The mailbox transfer object can only be used for one single mailbox transfer. If multiple transfers shall be initiated in parallel the client has to create one transfer object for each. The transfer object can be re-used after mailbox transfer completion.
Typical mailbox transfer sequence:
Record a mailbox transfer.
- Create a transfer object (for example an SDO download transfer object).
MbxTferDesc.dwMaxDataLen = 10 MbxTferDesc.pbyMbxTferDescData = (EC_T_PBYTE)OsMalloc(MbxTferDesc.dwMaxDataLen) pMbxTfer = emonMbxTferCreate(&MbxTferDesc) state of the transfer object = Idle
- Set the location to write the transferred data to, determine the transfer ID, store the client ID in the object and initiate the transfer (e.g. a SDO upload). A transfer may only be initiated if the state of the transfer object is Idle.
pMbxTfer->dwDataLen = MbxTferDesc.dwMaxDataLen; pMbxTfer->pbyMbxTferData = MbxTferDesc.pbyMbxTferDescData pMbxTfer->dwTferId = 1; pMbxTfer->dwClntId = dwClntId; dwResult = emonCoeSdoUplodadReq(pMbxTfer, dwSlaveId, wObIndex, ...); state of the transfer object = Pend or TferReqError
The state will then be set to Pend to indicate that this mailbox transfer object currently is in use and the transfer is not completed. If the mailbox transfer cannot be initiated the MainDevice will set the object into the state TferReqError - in such cases the client is responsible to set the state back into Idle.
- If the mailbox transfer is completed the notification callback function of the corresponding client (
emonNotify()) will be called with a pointer to the mailbox transfer object. The state of the transfer object is set to TferDone prior to callingemonNotify(). if( dwResult != EC_E_NOERROR ) { ... } emonNotify( EC_NOTIFY_MBOXRCV, pParms ) state of the transfer object = TferDone
- If the mailbox transfer is completed the notification callback function of the corresponding client (
- In case of errors the appropriate error handling has to be executed. The application must set the transfer object state to Idle.
if( pMbxTfer->dwErrorCode != EC_E_NOERROR ) { ... } In emonNotify: application may set transfer object state to Idle
- Delete the transfer object. Alternatively this object can be used for the next transfer.
emonMbxTferDelete(pMbxTfer);
9.7.1. Mailbox transfer object states
The following states exist for a mailbox transfer object:
A mailbox transfer will be processed by the monitor independently from the client’s timeout setting. Some types of mailbox transfers can be cancelled by the client, e.g. if the client’s timeout elapsed.
After completion of the mailbox transfer (with timeout) the client may finally set the transfer object into
the state EC_T_MBXTFER_STATUS::eMbxTferStatus_Idle.
New mailbox transfers can only be requested if the object is in the state EC_T_MBXTFER_STATUS::eMbxTferStatus_Idle.
9.7.2. emonMbxTferCreate
-
EC_T_MBXTFER *emonMbxTferCreate(EC_T_DWORD dwInstanceID, EC_T_MBXTFER_DESC *pMbxTferDesc)
Creates a mailbox transfer object.
While a mailbox transfer is in process the related transfer object and the corresponding memory may not be accessed. After a mailbox transfer completion the object may be used for the next transfer. The mailbox transfer object has to be deleted by calling ecatMbxTferDelete if it is not needed any more.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pMbxTferDesc – [in] Pointer to the mailbox transfer descriptor. Determines details of the mailbox transfer.
- Returns:
Pointer to the created mailbox transfer object if successful
EC_NULL on error (No memory left)
-
struct EC_T_MBXTFER_DESC
Public Members
-
EC_T_DWORD dwMaxDataLen
Maximum amount of data bytes that shall be transferred using this object. A mailbox transfer type without data transfer will ignore this parameter.
-
EC_T_BYTE *pbyMbxTferDescData
Pointer to byte stream carrying in and out data of mailbox content
-
EC_T_DWORD dwMaxDataLen
-
struct EC_T_MBXTFER
Public Members
-
EC_T_DWORD dwClntId
[] Client ID
-
EC_T_MBXTFER_DESC MbxTferDesc
[out] Mailbox transfer descriptor. All elements of pMbxTferDesc will be stored here.
-
EC_T_MBXTFER_TYPE eMbxTferType
[] This type of information is written to the Mailbox Transfer Object by the last call to a mailbox command function. It may be used as information, and is required to fan out consecutive notifications. This value is only valid until the next relevant mailbox API call, where this value may be overwritten.
-
EC_T_DWORD dwDataLen
[] Amount of data bytes for the next mailbox download transfer. If the mailbox transfer does not transfer data to the slave this parameter will be ignored. This element has to be set to an appropriate value every time prior to initiating a new download request. When either a download or upload transfer is completed (emNotify) this value will contain the amount of data that was actually transferred.
-
EC_T_BYTE *pbyMbxTferData
[in/out] Pointer to data. In case of a download transfer the client has to store the data in this location. In case of an upload transfer this element points to the received data. Access to data that was uploaded from a slave is only valid within the notification function because the buffer will be re-used by the master. These data have to be copied into a separate buffer in case it has to be used later by the client.
-
EC_T_MBXTFER_STATUS eTferStatus
[out] Transfer state. After a new transfer object is created the state will be set to eMbxTferStatus_Idle.
-
EC_T_DWORD dwErrorCode
[out] Error code of a mailbox transfer that was terminated with error
-
EC_T_DWORD dwTferId
[] Transfer ID. For every new mailbox transfer a unique ID has to be assigned. This ID can be used after mailbox transfer completion to identify the transfer.
-
EC_T_MBX_DATA MbxData
[] Mailbox data. This element contains mailbox transfer data, e.g. the CoE object dictionary list.
-
EC_T_DWORD dwClntId
-
union EC_T_MBX_DATA
- #include <EcInterfaceCommon.h>
Public Members
-
EC_T_MBX_DATA_COE CoE
CoE
-
EC_T_COE_ODLIST CoE_ODList
CoE Object Dictionary list
-
EC_T_COE_ENTRYDESC CoE_EntryDesc
CoE entry description
-
EC_T_COE_EMERGENCY CoE_Emergency
CoE emergency data
-
EC_T_MBX_DATA_FOE FoE
FoE
-
EC_T_MBX_DATA_FOE_REQ FoE_Request
FoE request
-
EC_T_MBX_DATA_COE CoE
9.7.3. emonMbxTferAbort
-
EC_T_DWORD emonMbxTferAbort(EC_T_DWORD dwInstanceID, EC_T_MBXTFER *pMbxTfer)
Abort a running mailbox transfer.
This function may not be called from within the JobTask’s context.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pMbxTfer – [in] Mailbox transfer object created with emMbxTferCreate
- Returns:
EC_E_NOERROR if successful
Currently only supported for FoE Transfer, CoE Download and CoE Upload.
9.7.4. emonMbxTferDelete
-
EC_T_VOID emonMbxTferDelete(EC_T_DWORD dwInstanceID, EC_T_MBXTFER *pMbxTfer)
Deletes a mailbox transfer object.
A transfer object may only be deleted if it is in the Idle state.
- Parameters:
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pMbxTfer – [in] Mailbox transfer object created with emMbxTferCreate
- Returns:
EC_E_NOERROR or error code
9.7.5. emonNotify - EC_NOTIFY_MBOXRCV
Indicates a mailbox transfer completion.
- emonNotify - EC_NOTIFY_MBOXRCV
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, containing the corresponding mailbox transfer objectdwInBufSize: [in] Size of the transfer object provided at pbyInBuf in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The element EC_T_MBXTFER::dwClntId contains the corresponding ID of the client that is notified, the corresponding transfer ID can be found in EC_T_MBXTFER::dwTferId. The transfer result is stored in EC_T_MBXTFER::dwErrorCode.
On error EC_T_MBXTFER::eTferStatus is eMbxTferStatus_TferReqError, on success eMbxTferStatus_TferDone. In order to reuse the transfer object the application must set it back to eMbxTferStatus_Idle.
The EC_T_MBXTFER::eMbxTferType element determines the mailbox transfer type (e.g. eMbxTferType_COE_SDO_DOWNLOAD for a completion of a CoE SDO download transfer).
9.7.6. emonNotify - EC_NOTIFY_COE_MBXSND_WKC_ERROR
Indicates a WKC error during a mailbox write. Detailed error information is stored in structure EC_T_WKCERR_DESC which is part of EC_T_ERROR_NOTIFICATION_DESC.
- emonNotify - EC_NOTIFY_COE_MBXSND_WKC_ERROR
- Parameter
pbyInBuf: [in] Pointer to EC_T_ERROR_NOTIFICATION_DESCdwInBufSize: [in] Size of the error description provided at pbyInBuf in bytespbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL