5.13. Texas Instruments ICSSG - emllICSSG on AM654x
The parameters to the ICSSG Link Layer are setup-specific. The function CreateLinkParmsFromCmdLineICSSG() in EcSelectLinkLayer.cpp demonstrates how to initialize the Link Layer instance.
-
struct EC_T_LINK_PARMS_ICSSG
Public Members
-
EC_T_LINK_PARMS linkParms
Common link parameters. Signature must be set to EC_LINK_PARMS_SIGNATURE_ICSSG
-
EC_T_LINK_ICSSG_BOARD eBoardType
TI System on Chip board type
-
EC_T_BOOL bMaster
Initialize whole PRUSS subsystem, not only port. This flag is always required when link layer is used on single ICSSG port. This flag is also required, when link layer is used in “Redundancy mode” and two ICSSG ports are used. In this case, first port should be master, and second port should be slave
-
EC_T_LINK_PARMS linkParms
5.13.1. TI AM654x IDK
Support for ICSSG on AM654x is currently limited to TI AM654x IDK/EVK with TI RTOS/Sysbios in polling mode.