6.11. CAN application protocol over EtherCAT (CoE)
6.11.1. emCoeSdoDownload
-
static EC_T_DWORD ecatCoeSdoDownload(EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_BYTE *pbyData, EC_T_DWORD dwDataLen, EC_T_DWORD dwTimeout, EC_T_DWORD dwFlags)
-
EC_T_DWORD emCoeSdoDownload(EC_T_DWORD dwInstanceID, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_BYTE *pbyData, EC_T_DWORD dwDataLen, EC_T_DWORD dwTimeout, EC_T_DWORD dwFlags)
Execute a CoE SDO download to an EtherCAT slave device.
This function may not be called from within the JobTask’s context.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwSlaveId – [in] Slave ID
wObIndex – [in] Object index.
byObSubIndex – [in] Object sub index. 0 or 1 if Complete Access.
pbyData – [in] Buffer containing transfered data
dwDataLen – [in] Buffer length [bytes]
dwTimeout – [in] Timeout [ms]
dwFlags – [in] Mailbox Flags. Bit 0: set if Complete Access (EC_MAILBOX_FLAG_SDO_COMPLETE).
- Returns
EC_E_NOERROR or error code
See also
6.11.2. emCoeSdoDownloadReq
-
static EC_T_DWORD ecatCoeSdoDownloadReq(EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_DWORD dwTimeout, EC_T_DWORD dwFlags)
-
EC_T_DWORD emCoeSdoDownloadReq(EC_T_DWORD dwInstanceID, EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_DWORD dwTimeout, EC_T_DWORD dwFlags)
Initiates a CoE SDO download to an EtherCAT slave device and returns immediately.
The length of the data to be downloaded must be set in EC_T_MBXTFER.dwDataLen. A unique transfer ID must be written into EC_T_MBXTFER.dwTferId. EC_NOTIFY_MBOXRCV is given on completion.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pMbxTfer – [in] Mailbox transfer object
dwSlaveId – [in] Slave ID
wObIndex – [in] Object index
byObSubIndex – [in] Object sub index. 0 or 1 if Complete Access.
dwTimeout – [in] Timeout [ms]
dwFlags – [in] Mailbox Flags. Bit 0: set if Complete Access (EC_MAILBOX_FLAG_SDO_COMPLETE).
- Returns
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if master isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range, the input pointer is EC_NULL or contains EC_NULL pointer, or dwTimeout is EC_NOWAIT
EC_E_NOMEMORY if the mailbox protocol queue of the slave if full
EC_E_SLAVE_NOT_PRESENT if slave not present
EC_E_NOTFOUND if no slave matching dwSlaveId can be found
EC_E_NO_MBX_SUPPORT if slave has no mailbox support
EC_E_INVALID_SLAVE_STATE if slave is in an invalid state for mailbox transfer
EC_E_MASTER_RED_STATE_INACTIVE if Master Redundancy is configured and master is inactive
EC_E_ADS_IS_RUNNING if ADS server is running
6.11.3. emNotify - eMbxTferType_COE_SDO_DOWNLOAD
SDO download transfer completion.
- emNotify - eMbxTferType_COE_SDO_DOWNLOAD
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, this structure contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The corresponding transfer ID can be found in EC_T_MBXTFER::dwTferId. The transfer result is stored in EC_T_MBXTFER::dwErrorCode.
The request parameters stored in element EC_T_MBX_DATA::CoE of type EC_T_MBX_DATA_COE are part of EC_T_MBXTFER::MbxData and may have to be buffered by the client.
Access to the memory area EC_T_MBXTFER::MbxData outside of the notification caller context is illegal and the results are undefined.
6.11.4. emCoeSdoUpload
-
static EC_T_DWORD ecatCoeSdoUpload(EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_BYTE *pbyData, EC_T_DWORD dwDataLen, EC_T_DWORD *pdwOutDataLen, EC_T_DWORD dwTimeout, EC_T_DWORD dwFlags)
-
EC_T_DWORD emCoeSdoUpload(EC_T_DWORD dwInstanceID, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_BYTE *pbyData, EC_T_DWORD dwDataLen, EC_T_DWORD *pdwOutDataLen, EC_T_DWORD dwTimeout, EC_T_DWORD dwFlags)
Execute a CoE SDO upload from an EtherCAT slave device to the master.
This function may not be called from within the JobTask’s context.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
dwSlaveId – [in] Slave ID
wObIndex – [in] Object index.
byObSubIndex – [in] Object sub index. 0 or 1 if Complete Access.
pbyData – [out] Buffer receiving transfered data
dwDataLen – [in] Buffer length [bytes]
pdwOutDataLen – [out] Length of received data [byte]
dwTimeout – [in] Timeout [ms]
dwFlags – [in] Mailbox Flags. Bit 0: set if Complete Access (EC_MAILBOX_FLAG_SDO_COMPLETE).
- Returns
EC_E_NOERROR or error code
See also
6.11.5. emCoeSdoUploadReq
-
static EC_T_DWORD ecatCoeSdoUploadReq(EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_DWORD dwTimeout, EC_T_DWORD dwFlags)
-
EC_T_DWORD emCoeSdoUploadReq(EC_T_DWORD dwInstanceID, EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_DWORD dwTimeout, EC_T_DWORD dwFlags)
Initiates a CoE SDO upload from an EtherCAT slave device to the master and returns immediately.
The length of the data to be uploaded must be set in EC_T_MBXTFER.dwDataLen. A unique transfer ID must be written into EC_T_MBXTFER.dwTferId. EC_NOTIFY_MBOXRCV is given on completion.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pMbxTfer – [in] Mailbox transfer object created with emMbxTferCreate
dwSlaveId – [in] Slave ID
wObIndex – [in] Object index
byObSubIndex – [in] Object sub index. 0 or 1 if Complete Access.
dwTimeout – [in] Timeout [ms]
dwFlags – [in] Mailbox Flags. Bit 0: set if Complete Access (EC_MAILBOX_FLAG_SDO_COMPLETE).
- Returns
EC_E_NOERROR if successful
EC_E_INVALIDSTATE if master isn’t initialized
EC_E_INVALIDPARM if dwInstanceID is out of range, the input pointer is EC_NULL or contains EC_NULL pointer, or dwTimeout is EC_NOWAIT
EC_E_NOMEMORY if the mailbox protocol queue of the slave if full
EC_E_SLAVE_NOT_PRESENT if slave not present
EC_E_NOTFOUND if no slave matching dwSlaveId can be found
EC_E_NO_MBX_SUPPORT if slave has no mailbox support
EC_E_INVALID_SLAVE_STATE if slave is in an invalid state for mailbox transfer
EC_E_MASTER_RED_STATE_INACTIVE if Master Redundancy is configured and master is inactive
EC_E_ADS_IS_RUNNING if ADS server is running
Example
The following code demonstrates how to upload a CoE object from a slave using the non-blocking API emCoeSdoUploadReq().
In this example the mailbox transfer object state is polled. emNotify - EC_NOTIFY_MBOXRCV can be used as alternative to polling.
EC_T_DWORD CoeSdoUploadReqExample()
{
EC_T_DWORD dwRetVal = EC_E_ERROR;
EC_T_DWORD dwRes = EC_E_ERROR;
/* needed only for notifications, see
- ecatRegisterClient(...)
- pAppContext->pNotificationHandler->GetClientID() */
EC_T_DWORD dwClientId = 0;
/* slave with station address 2002 used for CoE SDO upload */
EC_T_DWORD dwSlaveId = ecatGetSlaveId(2002);
EC_T_MBXTFER* pMbxTferObject = EC_NULL;
EC_T_BYTE abyObjectDataBuffer[] = { 0, 0, 0, 0 };
EC_T_MBXTFER_DESC oObjectDataTferDesc;
OsMemset(&oObjectDataTferDesc, 0, sizeof(EC_T_MBXTFER_DESC));
/* create mailbox transfer object */
oObjectDataTferDesc.pbyMbxTferDescData = abyObjectDataBuffer;
oObjectDataTferDesc.dwMaxDataLen = sizeof(abyObjectDataBuffer);
pMbxTferObject = ecatMbxTferCreate(&oObjectDataTferDesc);
if (EC_NULL == pMbxTferObject)
{
dwRes = EC_E_NOMEMORY;
dwRetVal = dwRes;
goto Exit;
}
/* create mailbox transfer object */
pMbxTferObject->dwClntId = dwClientId;
pMbxTferObject->dwTferId = 1; /* assigned by application. should be unique for each object */
/* request upload of object index 0x1018, subindex 1, timeout 5s, no complete access */
dwRes = ecatCoeSdoUploadReq(pMbxTferObject, dwSlaveId, 0x1018, 1, 5000, 0);
if (EC_E_NOERROR != dwRes)
{
dwRetVal = dwRes;
goto Exit;
}
/* wait for transfer finished */
while (eMbxTferStatus_Pend == pMbxTferObject->eTferStatus)
{
OsSleep(10);
/* transfer can be canceled using ecatMbxTferAbort(...) if it takes too long */
}
/* check transfer result */
dwRes = pMbxTferObject->dwErrorCode;
if (EC_E_NOERROR != dwRes)
{
dwRetVal = dwRes;
goto Exit;
}
dwRetVal = EC_E_NOERROR;
Exit:
if (EC_NULL != pMbxTferObject)
{
pMbxTferObject->eTferStatus = eMbxTferStatus_Idle;
ecatMbxTferDelete(pMbxTferObject);
}
return dwRetVal;
}
6.11.6. emNotify - eMbxTferType_COE_SDO_UPLOAD
SDO upload transfer completion.
- emNotify - eMbxTferType_COE_SDO_UPLOAD
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The corresponding transfer ID can be found in EC_T_MBXTFER::dwTferId. The transfer result is stored in EC_T_MBXTFER::dwErrorCode.
The request parameters stored in element EC_T_MBX_DATA::CoE of type EC_T_MBX_DATA_COE are part of EC_T_MBXTFER::MbxData.
The SDO data stored in EC_T_MBXTFER::pbyMbxTferData may have to be buffered by the client.
Access to the memory area referenced by EC_T_MBXTFER::pbyMbxTferData outside of the notification caller context is illegal and the results are undefined.
6.11.7. emCoeGetODList
-
static EC_T_DWORD ecatCoeGetODList(EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_COE_ODLIST_TYPE eListType, EC_T_DWORD dwTimeout)
-
EC_T_DWORD emCoeGetODList(EC_T_DWORD dwInstanceID, EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_COE_ODLIST_TYPE eListType, EC_T_DWORD dwTimeout)
Gets a list of object IDs that are available in a slave.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pMbxTfer – [in] Mailbox transfer
dwSlaveId – [in] Slave ID
eListType – [in] which object types shall be transferred
dwTimeout – [in] Timeout [ms] The function will block at most for this time. If the timeout value is set to EC_NOWAIT the function will return immediately.
6.11.8. emNotify - eMbxTferType_COE_GETODLIST
Object dictionary list upload transfer completion.
- emNotify - eMbxTferType_COE_GETODLIST
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The corresponding transfer ID can be found in EC_T_MBXTFER::dwTferId. The transfer result is stored in EC_T_MBXTFER::dwErrorCode.
The object list stored in element EC_T_MBX_DATA::CoE_ODList of type EC_T_COE_ODLIST is part of EC_T_MBXTFER::MbxData and may have to be buffered by the client.
Access to the memory area EC_T_MBXTFER::MbxData outside of the notification caller context is illegal and the results are undefined.
-
struct EC_T_COE_ODLIST
Public Members
-
EC_T_COE_ODLIST_TYPE eOdListType
list type
-
EC_T_COE_ODLIST_TYPE eOdListType
6.11.9. emCoeGetObjectDesc
-
static EC_T_DWORD ecatCoeGetObjectDesc(EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_DWORD dwTimeout)
-
EC_T_DWORD emCoeGetObjectDesc(EC_T_DWORD dwInstanceID, EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_DWORD dwTimeout)
Determines the description of a specific object.
A unique transfer ID must be written into EC_T_MBXTFER.dwTferId. EC_NOTIFY_MBOXRCV is given on completion. This function may not be called from within the JobTask’s context.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pMbxTfer – [in] Mailbox transfer object
dwSlaveId – [in] Slave ID
wObIndex – [in] Object index
dwTimeout – [in] Timeout [ms] The function will block at most for this time. If the timeout value is set to EC_NOWAIT the function will return immediately.
- Returns
EC_E_NOERROR or error code
6.11.10. emNotify - eMbxTferType_COE_GETOBDESC
Completion of a SDO information service transfer to get a object description.
- emNotify - eMbxTferType_COE_GETOBDESC
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The corresponding transfer ID can be found in EC_T_MBXTFER::dwTferId. The transfer result is stored in EC_T_MBXTFER::dwErrorCode.
The object description stored in element EC_T_MBX_DATA::CoE_ObDesc of type EC_T_COE_OBDESC is part of EC_T_MBXTFER::MbxData and may have to be buffered by the client.
Access to the memory area EC_T_MBXTFER::MbxData outside of the notification caller context is illegal and the results are undefined.
See also
A more detailed description of the values for data type, object code etc. can be found in the EtherCAT specification ETG.1000, section 5.
6.11.11. emCoeGetEntryDesc
-
static EC_T_DWORD ecatCoeGetEntryDesc(EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_BYTE byValueInfo, EC_T_DWORD dwTimeout)
-
EC_T_DWORD emCoeGetEntryDesc(EC_T_DWORD dwInstanceID, EC_T_MBXTFER *pMbxTfer, EC_T_DWORD dwSlaveId, EC_T_WORD wObIndex, EC_T_BYTE byObSubIndex, EC_T_BYTE byValueInfo, EC_T_DWORD dwTimeout)
Determines the description of a specific object entry.
A unique transfer ID must be written into EC_T_MBXTFER.dwTferId. EC_NOTIFY_MBOXRCV is given on completion. This function may not be called from within the JobTask’s context.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
pMbxTfer – [in] Mailbox transfer object
dwSlaveId – [in] Slave ID
wObIndex – [in] Object index
byObSubIndex – [in] Object sub-index
byValueInfo – [in] The value info bit mask includes which elements shall be in the response. See Value info flags for available values.
dwTimeout – [in] Timeout [ms] The function will block at most for this time. If the timeout value is set to EC_NOWAIT the function will return immediately
- Returns
EC_E_NOERROR or error code
Value info flags
- group EC_COE_ENTRY_VALUEINFO
EtherCat CoE entry description value information bit definitions
6.11.12. emNotify - eMbxTferType_COE_GETENTRYDESC
Completion of a SDO information service transfer to get a object entry description.
- emNotify - eMbxTferType_COE_GETENTRYDESC
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The corresponding transfer ID can be found in EC_T_MBXTFER::dwTferId. The transfer result is stored in EC_T_MBXTFER::dwErrorCode.
The object entry description stored in element EC_T_MBX_DATA::CoE_EntryDesc of type EC_T_COE_ENTRYDESC is part of EC_T_MBXTFER::MbxData and may have to be buffered by the client.
Access to the memory area EC_T_MBXTFER::MbxData outside of the notification caller context is illegal and the results are undefined.
-
struct EC_T_COE_ENTRYDESC
Public Members
-
EC_T_BYTE byValueInfo
Bit mask which information is included in pbyData. See Value info flags
-
EC_T_BYTE byObAccess
Access rights. See Object access flags
-
EC_T_BYTE byValueInfo
Object access flags
- group EC_COE_ENTRY_OBJACCESS
EtherCat CoE entry access bit definitions
Defines
See also
A example for the evaluation of
EC_T_COE_ENTRYDESC::pbyDatacomes with EcMasterDemo.A more detailed description of the values can be found in the EtherCAT specification ETG.1000, section 5 and 6.
6.11.13. emCoeProfileGetChannelInfo
-
static EC_T_DWORD ecatCoeProfileGetChannelInfo(EC_T_BOOL bStationAddress, EC_T_WORD wSlaveAddress, EC_T_DWORD dwChannel, EC_T_PROFILE_CHANNEL_INFO *pInfo)
-
EC_T_DWORD emCoeProfileGetChannelInfo(EC_T_DWORD dwInstanceID, EC_T_BOOL bFixedAddressing, EC_T_WORD wSlaveAddress, EC_T_DWORD dwChannel, EC_T_PROFILE_CHANNEL_INFO *pInfo)
Return information about a configured CoE profile channel from the ENI file.
- Parameters
dwInstanceID – [in] Instance ID (Multiple EtherCAT Network Support)
bFixedAddressing – [in] EC_TRUE: use station address, EC_FALSE: use AutoInc address
wSlaveAddress – [in] Slave address according bFixedAddressing
dwChannel – [in] Channel
pInfo – [out] Channel info
- Returns
EC_E_NOERROR or error code
6.11.14. emNotify - EC_NOTIFY_COE_INIT_CMD
Indicates a COE mailbox transfer completion during slave state transition. This notification is disabled by default.
- emNotify - EC_NOTIFY_COE_INIT_CMD
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object provided at pbyInBuf in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
The EC_T_MBX_DATA::CoE_InitCmd element of type EC_T_MBX_DATA_COE_INITCMD is part of EC_T_MBXTFER::MbxData and may have to be buffered by the client.
Access to the memory area EC_T_MBXTFER::MbxData outside of the notification caller context is illegal and the results are undefined.
-
struct EC_T_MBX_DATA_COE_INITCMD
Public Members
-
EC_T_SLAVE_PROP SlaveProp
Slave properties
-
EC_T_SLAVE_PROP SlaveProp
6.11.15. CoE Emergency (emNotify - eMbxTferType_COE_EMERGENCY)
Indication of a CoE emergency request. A emNotify - EC_NOTIFY_MBOXRCV is given with EC_T_MBXTFER::eMbxTferType = EC_T_MBXTFER_TYPE::eMbxTferType_COE_EMERGENCY.
- emNotify - eMbxTferType_COE_EMERGENCY
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
In case of an emergency notification all registered clients will get this notification.
The corresponding mailbox transfer object will be created inside the EtherCAT master. The content in EC_T_MBXTFER::dwTferId is undefined as it is not needed by the client and the master.
The transfer result is stored in EC_T_MBXTFER::dwErrorCode.
The emergency data stored in element EC_T_MBX_DATA::CoE_Emergency of type EC_T_COE_EMERGENCY is part of EC_T_MBXTFER::MbxData and may have to be buffered by the client.
Access to the memory area EC_T_MBXTFER::MbxData outside of the notification caller context is illegal and the results are undefined.
See also
A more detailed description of the values can be found in the EtherCAT specification ETG.1000, section 5.
6.11.16. CoE Abort (emNotify - EC_NOTIFY_MBSLAVE_COE_SDO_ABORT)
The application can abort asynchronous CoE Uploads and Downloads.
The slave may abort CoE Uploads and Downloads which is indicated at the return code of emCoeSdoUpload(), … .
This notification is given if an SDO transfer aborts while sending init commands.
- emNotify - EC_NOTIFY_MBSLAVE_COE_SDO_ABORT
- Parameter
pbyInBuf: [in] Pointer to a structure of type EC_T_MBXTFER, contains the corresponding mailbox transfer object.dwInBufSize: [in] Size of the transfer object in bytes.pbyOutBuf: [out] Should be set to EC_NULLdwOutBufSize: [in] Should be set to 0pdwNumOutData: [out] Should be set to EC_NULL
Detailed error information is stored in structure EC_T_MBOX_SDO_ABORT_DESC of the union element SdoAbortDesc.
-
struct EC_T_MBOX_SDO_ABORT_DESC
Public Members
-
EC_T_SLAVE_PROP SlaveProp
Slave properties
-
EC_T_SLAVE_PROP SlaveProp
See also
6.11.17. emConvertEcErrorToCoeError
-
EC_T_DWORD emConvertEcErrorToCoeError(EC_T_DWORD dwInstanceID, EC_T_DWORD dwErrorCode)
Convert master error code to CoE error code.
- Returns
CoE error code according to the following specifications:
CoE Abort Codes defined in ETG.1000.6 V1.0.4, Table 41: SDO Abort Codes
Additional codes defined in ETG.1020, V1.2.0, Table 21: CoE Abort Codes (extension)