8. Error Codes
8.1. Groups
No. |
Group |
Abbr. |
Description |
|---|---|---|---|
1 |
Application Error |
APP |
Error within application, running the master E.g. API function call with invalid parameters |
2 |
EtherCAT network information file problem |
ENI |
Master configuration XML file mismatches slave configuration on bus E.g. Bus Topology Scan cannot detect all slaves configured within network information file |
3 |
Master parameter configuration |
CFG |
Master configuration parameters erroreous E.g. mailbox command queue not large enough |
4 |
Bus/Slave Error |
SLV |
Slave error E.g. Working Counter Error |
5 |
Link Layer |
LLA |
Link Layer errror (network interface driver) E.g. Intel Pro/1000 NIC could not be found |
6 |
Remote API |
RAS |
Remote API error E.g. connection to Remote API server is not possible from client |
7 |
Internal software error |
ISW |
Master internal error E.g. Master state machine in undefined state |
8 |
DC Master Sync |
DCM |
DC slave and host time synchronization |
9 |
Pass-Through-Server |
PTS |
Initialisation/De-Initialisation errors |
10 |
System Setup |
SYS |
Errors from Operating System or obviously due to System Setup |
8.2. Generic Error Codes
-
EC_E_INVALIDOFFSET
0x98110003: ISW: Invalid offset (e.g. invalid offset while accessing Process Data Image)
-
EC_E_BUSY
0x98110008: APP: Busy (e.g. stack is busy currently and not available to process the API request. The function may be called again later)
-
EC_E_ACYC_FRM_FREEQ_EMPTY
0x98110009: ISW: Cannot queue acyclic EtherCAT command (Acyclic command queue is full. Possible solution: Increase of configuration value dwMaxQueuedEthFrames)
-
EC_E_INVALIDPARM
0x9811000B: APP: Invalid parameter (e.g. API function called with erroneous parameter set)
-
EC_E_NOTFOUND
0x9811000C: APP: Not found (e.g. Network Information File ENI not found or API called with invalid slave ID)
-
EC_E_UNKNOWN_MBX_PROTOCOL
0x98110015: ISW: Unknown Mailbox Protocol Command (Unknown Mailbox protocol or mailbox command with unknown protocol association)
-
EC_E_IDENTIFICATIONFAILED
0x98110017: ENI: Identification failed (e.g. identification command failed)
-
EC_E_PRODKEY_INVALID
0x9811001A: CFG: Product Key Invalid (e.g. application using protected version of the stack, which stops operation after the evaluation time limit reached if a license is not provided)
-
EC_E_WRONG_FORMAT
0x9811001B: ENI: Wrong configuration format (e.g. Network information file empty or malformed)
-
EC_E_FEATURE_DISABLED
0x9811001C: APP: Feature disabled (e.g. Application tried to perform a missing or disabled API function)
-
EC_E_BUSCONFIG_MISMATCH
0x9811001E: ENI: Bus configuration mismatch (e.g. Network information file and currently connected bus topology does not match)
-
EC_E_CONFIGDATAREAD
0x9811001F: ENI: Error reading configuration file (e.g. Network information file could not be read)
-
EC_E_ENI_NO_SAFEOP_OP_SUPPORT
0x98110020: Configuration doesn’t support SAFEOP and OP requested state
-
EC_E_XML_CYCCMDS_MISSING
0x98110021: ENI: Cyclic commands are missing (e.g. Network information file does not contain cyclic commands)
-
EC_E_XML_ALSTATUS_READ_MISSING
0x98110022: ENI: AL_STATUS register read missing in XML file for at least one state (e.g. Read of AL Status register is missing in cyclic part of given network information file)
-
EC_E_MCSM_FATAL_ERROR
0x98110023: ISW: Fatal internal McSm (master control state machine is in an undefined state)
-
EC_E_SLAVE_ERROR
0x98110024: SLV: Slave error (e.g. A slave error was detected. See also EC_NOTIFY_STATUS_SLAVE_ERROR and EC_NOTIFY_SLAVE_ERROR_STATUS_INFO)
-
EC_E_FRAME_LOST
0x98110025: SLV: Frame lost, IDX mismatch (EtherCAT frame(s) lost on bus, means the response was not received. In case this error shows frequently a problem with the wiring could be the cause)
-
EC_E_CMD_MISSING
0x98110026: SLV: At least one EtherCAT command is missing in the received frame (e.g. received EtherCAT frame incomplete)
-
EC_E_INVALID_DCL_MODE
0x98110028: APP: IOCTL EC_IOCTL_DC_LATCH_REQ_LTIMVALS invalid in DCL auto read mode (this function cannot be used if DC Latching is running in mode “Auto Read”)
-
EC_E_AI_ADDRESS
0x98110029: SLV: Auto increment address increment mismatch (e.g. Network information file and bus topology doesn’t match any more. Error shows only, if a already recognized slave isn’t present any more)
-
EC_E_INVALID_SLAVE_STATE
0x9811002A: APP: Slave in invalid state, e.g. not in OP (API not callable in this state) (mailbox commands are not allowed in current slave state)
-
EC_E_SLAVE_NOT_ADDRESSABLE
0x9811002B: SLV: Station address lost (or slave missing) - FPRD to AL_STATUS failed (e.g. Slave had a power cycle)
-
EC_E_CYC_CMDS_OVERFLOW
0x9811002C: ENI: Too many cyclic commands in XML configuration file (e.g. EC_T_INIT_MASTER_PARMS.dwMaxAcycFramesQueued too small)
-
EC_E_LINK_DISCONNECTED
0x9811002D: SLV: Ethernet link cable disconnected (e.g. EtherCAT bus segment not connected to network interface)
-
EC_E_MASTERCORE_INACCESSIBLE
0x9811002E: RAS: Master core not accessible (e.g. Connection to remote server was terminated or master instance has been stopped on remote side)
-
EC_E_COE_MBXSND_WKC_ERROR
0x9811002F: SLV: CoE mailbox send: working counter (e.g. CoE mailbox couldn’t be read on slave, slave didn’t read out mailbox since last write)
-
EC_E_COE_MBXRCV_WKC_ERROR
0x98110030: SLV: CoE mailbox receive: working counter (e.g. CoE mailbox couldn’t be read from slave)
-
EC_E_NO_MBX_SUPPORT
0x98110031: APP: No mailbox support (e.g. Slave does not support mailbox access)
-
EC_E_NO_COE_SUPPORT
0x98110032: ENI: CoE protocol not supported (e.g. Configuration error or slave information file doesn’t match slave firmware)
-
EC_E_NO_EOE_SUPPORT
0x98110033: ENI: EoE protocol not supported (e.g. Configuration error or slave information file doesn’t match slave firmware)
-
EC_E_NO_FOE_SUPPORT
0x98110034: ENI: FoE protocol not supported (e.g. Configuration error or slave information file doesn’t match slave firmware)
-
EC_E_NO_SOE_SUPPORT
0x98110035: ENI: SoE protocol not supported (e.g. Configuration error or slave information file doesn’t match slave firmware)
-
EC_E_NO_VOE_SUPPORT
0x98110036: ENI: VoE protocol not supported (e.g. Configuration error or slave information file doesn’t match slave firmware)
-
EC_E_EVAL_EXPIRED
0x98110038: CFG: Evaluation Time limit reached (e.g. License not provided and evaluation period (1 hour) of protected version exceeded)
-
EC_E_CFGFILENOTFOUND
0x98110070: CFG: Master configuration not found (e.g. path to master configuration file (XML) was wrong or the file is not available)
-
EC_E_XML_CYCCMDS_SIZEMISMATCH
0x98110073: ENI: Cyclic command wrong size (too long) (size in master configuration file (XML) does not match size of process data)
-
EC_E_XML_INVALID_INP_OFF
0x98110074: ENI: Invalid input offset in cyclic command, please check InputOffs
-
EC_E_XML_INVALID_OUT_OFF
0x98110075: ENI: Invalid output offset in cyclic command, please check OutputOffs
-
EC_E_SLAVE_NOT_PRESENT
0x9811010E: APP / SLV: command not executed (slave not present on bus) (e.g. slave disappeared or was never present)
-
EC_E_SYSDRIVERMISSING
0x98110112: SYS: Cannot open system driver (e.g. system driver was not loaded)
-
EC_E_BUSCONFIG_TOPOCHANGE
0x9811011E: Bus configuration not detected, Topology changed (e.g. Topology changed while scanning bus)
-
EC_E_VOE_MBX_WKC_ERROR
0x98110123: SLV: VoE mailbox send: working counter (VoE mailbox couldn’t be written)
-
EC_E_REDLINEBREAK
0x98110126: SLV: Redundancy line break (e.g. cable break between slaves or between master and first slave)
-
EC_E_XML_INVALID_CMD_WITH_RED
0x98110127: ENI: Invalid EtherCAT command in cyclic frame with redundancy (e.g. BRW commands are not allowed with redundancy)
-
EC_E_XML_PREV_PORT_MISSING
0x98110128: ENI: <PreviousPort>-tag is missing (e.g. if the auto increment address is not the first slave on the bus we check if a previous port tag OR a hot connect tag is available)
-
EC_E_XML_DC_CYCCMDS_MISSING
0x98110129: DC enabled and DC cyclic commands missing (e.g. access to 0x0900)
-
EC_E_DLSTATUS_IRQ_TOPOCHANGED
0x98110130: SLV: Data link (DL) status interrupt because of changed topology (automatically handled by master)
-
EC_E_PTS_IS_NOT_RUNNING
0x98110131: PTS: Pass Through Server is not running (Pass-Through-Server was tried to be enabled/disabled or stopped without being started)
-
EC_E_PTS_IS_RUNNING
0x98110132: PTS: Pass Through Server is running (obsolete, replaced by EC_E_ADS_IS_RUNNING)
-
EC_E_ADS_IS_RUNNING
0x98110132: PTS: ADS adapter (Pass Through Server) is running (API call conflicts with ADS state (running))
-
EC_E_PTS_SOCK_BIND_FAILED
0x98110134: PTS: The Pass Through Server could not bind the IP address with a socket (e.g. Possibly because the IPaddress (and Port) is already in use or the IP-address does not exist)
-
EC_E_PTS_LL_MODE_NOT_SUPPORTED
0x98110136: PTS: The Link Layer mode is not supported by the Pass Through Server (e.g. The Master is running in interrupt mode but the Pass-Through-Server only supports polling mode)
-
EC_E_DC_REF_CLOCK_SYNC_OUT_UNIT_DISABLED
0x98110138: DC (time loop control) unit of reference clock disabled
-
EC_E_DC_REF_CLOCK_NOT_FOUND
0x98110139: SLV: Reference clock not found! May happen if reference clock is removed from network.
-
EC_E_MBX_CMD_WKC_ERROR
0x9811013B: SLV: Mailbox command working counter error (e.g. Mailbox init command Retry Count exceeded)
-
EC_E_NO_AOE_SUPPORT
0x9811013C: APP / SLV: AoE: Protocol not supported (e.g. Application calls AoE-API although not implemented at slave)
-
EC_E_MAX_BUS_SLAVES_EXCEEDED
0x9811016F: CFG: Error: Maximum number of bus slave has been exceeded (The maximum number of preallocated bus slave objects are to small. The maximum number can be adjusted by the master initialization parameter EC_T_INITMASTERPARMS.dwMaxBusSlaves)
-
EC_E_MBXERR_SYNTAX
0x98110170: SLV: Mailbox error: Syntax of 6 octet Mailbox header is wrong (Slave error mailbox return value: 0x01)
-
EC_E_MBXERR_UNSUPPORTEDPROTOCOL
0x98110171: SLV: Mailbox error: The Mailbox protocol is not supported (Slave error mailbox return value: 0x02)
-
EC_E_MBXERR_INVALIDCHANNEL
0x98110172: SLV: Mailbox error: Field contains wrong value (Slave error mailbox return value: 0x03)
-
EC_E_MBXERR_SERVICENOTSUPPORTED
0x98110173: SLV: Mailbox error: The mailbox protocol header of the mailbox protocol is wrong (Slave error mailbox return value: 0x04)
-
EC_E_MBXERR_INVALIDHEADER
0x98110174: SLV: Mailbox error: The mailbox protocol header of the mailbox protocol is wrong (Slave error mailbox return value: 0x05)
-
EC_E_MBXERR_SIZETOOSHORT
0x98110175: SLV: Mailbox error: Length of received mailbox data is too short (Slave error mailbox return value: 0x06)
-
EC_E_MBXERR_NOMOREMEMORY
0x98110176: SLV: Mailbox error: Mailbox protocol can not be processed because of limited resources (Slave error mailbox return value: 0x07)
-
EC_E_MBXERR_INVALIDSIZE
0x98110177: SLV: Mailbox error: The length of data is inconsistent (Slave error mailbox return value: 0x08)
-
EC_E_DC_SLAVES_BEFORE_REF_CLOCK
0x98110178: ENI: Slaves with DC configured present on bus before reference clock (e.g. The first DC Slave was not configured as potential reference clock)
-
EC_E_ADO_NOT_SUPPORTED
0x9811017E: SLV: ADO for slave identification not supported (e.g. Request ID mechanism (ADO 0x134) not supported by slave)
-
EC_E_ENI_ENCRYPTION_WRONG_VERSION
0x98130009: ENI, OEM: ENI encryption algorithm version not supported
-
EC_E_OEM_KEY_MISSING
0x9813000C: APP: OEM key access needs OEM key set (e.g. Application must call esSetOemKey (HiL) or set EC_T_LINK_PARMS_SIMULATOR::qwOemKey (SiL))
-
EC_E_MASTER_RED_STATE_INACTIVE
0x98130024: APP: Master Redundancy State is INACTIVE (e.g. API not allowed in current Master Redundancy State)
8.3. DCM Error Codes
8.4. ADS over EtherCAT (AoE) Error Codes
8.5. CAN application protocol over EtherCAT (CoE) SDO Error Codes
-
EC_E_SDO_ABORTCODE_TOGGLE
0x98110040: SLV: SDO: Toggle bit not alternated (CoE abort code 0x05030000 of slave)
-
EC_E_SDO_ABORTCODE_TIMEOUT
0x98110041: SLV: SDO: Protocol timed out (CoE abort code 0x05040000 of slave)
-
EC_E_SDO_ABORTCODE_CCS_SCS
0x98110042: SLV: SDO: Client/server command specifier not valid or unknown (CoE abort code 0x05040001 of slave)
-
EC_E_SDO_ABORTCODE_BLK_SIZE
0x98110043: SLV: SDO: Invalid block size (block mode only) (CoE abort code 0x05040002 of slave)
-
EC_E_SDO_ABORTCODE_SEQNO
0x98110044: SLV: SDO: Invalid sequence number (block mode only) (CoE abort code 0x05040003 of slave)
-
EC_E_SDO_ABORTCODE_CRC
0x98110045: SLV: SDO: CRC error (block mode only) (CoE abort code 0x05040004 of slave)
-
EC_E_SDO_ABORTCODE_ACCESS
0x98110047: SLV: SDO: Unsupported access to an object (CoE abort code 0x06010000 of slave)
-
EC_E_SDO_ABORTCODE_WRITEONLY
0x98110048: SLV: SDO: Attempt to read a write only object (CoE abort code 0x06010001 of slave)
-
EC_E_SDO_ABORTCODE_READONLY
0x98110049: SLV: SDO: Attempt to write a read only object (CoE abort code 0x06010002 of slave)
-
EC_E_SDO_ABORTCODE_INDEX
0x9811004A: SLV: SDO: Object does not exist in the object dictionary (CoE abort code 0x06020000 of slave)
-
EC_E_SDO_ABORTCODE_PDO_MAP
0x9811004B: SLV: SDO: Object cannot be mapped to the PDO (CoE abort code 0x06040041 of slave)
-
EC_E_SDO_ABORTCODE_PDO_LEN
0x9811004C: SLV: SDO: The number and length of the objects to be mapped would exceed PDO length (CoE abort code 0x06040042 of slave)
-
EC_E_SDO_ABORTCODE_P_INCOMP
0x9811004D: SLV: SDO: General parameter incompatibility reason (CoE abort code 0x06040043 of slave)
-
EC_E_SDO_ABORTCODE_I_INCOMP
0x9811004E: SLV: SDO: General internal incompatibility in the device (CoE abort code 0x06040047 of slave)
-
EC_E_SDO_ABORTCODE_HARDWARE
0x9811004F: SLV: SDO: Access failed due to an hardware error (CoE abort code 0x06060000 of slave)
-
EC_E_SDO_ABORTCODE_DATA_LENGTH_NOT_MATCH
0x98110050: SLV: SDO: Data type does not match, length of service parameter does not match (CoE abort code 0x06070010 of slave)
-
EC_E_SDO_ABORTCODE_DATA_LENGTH_TOO_HIGH
0x98110051: SLV: SDO: Data type does not match, length of service parameter too high (CoE abort code 0x06070012 of slave)
-
EC_E_SDO_ABORTCODE_DATA_LENGTH_TOO_LOW
0x98110052: SLV: SDO: Data type does not match, length of service parameter too low (CoE abort code 0x06070013 of slave)
-
EC_E_SDO_ABORTCODE_OFFSET
0x98110053: SLV: SDO: Sub-index does not exist (CoE abort code 0x06090011 of slave)
-
EC_E_SDO_ABORTCODE_VALUE_RANGE
0x98110054: SLV: SDO: Value range of parameter exceeded (only for write access) (CoE abort code 0x06090030 of slave)
-
EC_E_SDO_ABORTCODE_VALUE_TOO_HIGH
0x98110055: SLV: SDO: Value of parameter written too high (CoE abort code 0x06090031 of slave)
-
EC_E_SDO_ABORTCODE_VALUE_TOO_LOW
0x98110056: SLV: SDO: Value of parameter written too low (CoE abort code 0x06090032 of slave)
-
EC_E_SDO_ABORTCODE_MINMAX
0x98110057: SLV: SDO: Maximum value is less than minimum value (CoE abort code 0x06090036 of slave)
-
EC_E_SDO_ABORTCODE_TRANSFER
0x98110059: SLV: SDO: Data cannot be transferred or stored to the application (CoE abort code 0x08000020 of slave)
-
EC_E_SDO_ABORTCODE_TRANSFER_LOCAL_CONTROL
0x9811005A: SLV: SDO: Data cannot be transferred or stored to the application because of local control (CoE abort code 0x08000021 of slave)
-
EC_E_SDO_ABORTCODE_TRANSFER_DEVICE_STATE
0x9811005B: SLV: SDO: Data cannot be transferred or stored to the application because of the present device state (CoE abort code 0x08000022 of slave)
-
EC_E_SDO_ABORTCODE_DICTIONARY
0x9811005C: SLV: SDO: Object dictionary dynamic generation fails or no object dictionary is present (e.g. object dictionary is generated from file and generation fails because of an file error) (CoE abort code 0x08000023 of slave)
-
EC_E_SDO_ABORTCODE_MODULE_ID_LIST_NOT_MATCH
0x9811005E: Detected Module Ident List (0xF030) and Configured Module Ident list (0xF050) does not match
-
EC_E_SDO_ABORTCODE_SI_NOT_WRITTEN
0x98130004: SLV: SDO: Sub Index cannot be written, SI0 must be 0 for write access (CoE abort code 0x06010003 of slave)
-
EC_E_SDO_ABORTCODE_CA_TYPE_MISM
0x98130005: SLV: SDO: Complete access not supported for objects of variable length such as ENUM object types (CoE abort code 0x06010004 of slave)
8.6. File Transfer over EtherCAT (FoE) Error Codes
-
EC_E_FOE_ERRCODE_NOTDEFINED
0x98110060: SLV: ERROR FoE: not defined (FoE Error Code 0 (0x8000) of slave)
-
EC_E_FOE_ERRCODE_NOTFOUND
0x98110061: SLV: ERROR FoE: not found (FoE Error Code 1 (0x8001) of slave)
-
EC_E_FOE_ERRCODE_ACCESS
0x98110062: SLV: ERROR FoE: access denied (FoE Error Code 2 (0x8002) of slave)
-
EC_E_FOE_ERRCODE_DISKFULL
0x98110063: SLV: ERROR FoE: disk full (FoE Error Code 3 (0x8003) of slave)
-
EC_E_FOE_ERRCODE_PACKENO
0x98110065: SLV: ERROR FoE: packet number wrong (FoE Error Code 5 (0x8005) of slave)
-
EC_E_FOE_ERRCODE_EXISTS
0x98110066: SLV: ERROR FoE: already exists (FoE Error Code 6 (0x8006) of slave)
-
EC_E_FOE_ERRCODE_BOOTSTRAPONLY
0x98110068: SLV: ERROR FoE: bootstrap only (FoE Error Code 8 (0x8008) of slave)
-
EC_E_FOE_ERRCODE_NOTINBOOTSTRAP
0x98110069: SLV: ERROR FoE: Downloaded file name is not valid in Bootstrap state (FoE Error Code 9 (0x8009) of slave)
-
EC_E_FOE_ERRCODE_INVALIDPASSWORD
0x9811006A: SLV: ERROR FoE: no rights (FoE Error Code 10 (0x800A) of slave)
-
EC_E_FOE_ERRCODE_PROGERROR
0x9811006B: SLV: ERROR FoE: program error (FoE Error Code 11 (0x800B) of slave)
-
EC_E_FOE_ERRCODE_INVALID_FIRMWARE
0x9811006D: SLV: ERROR FoE: Firmware does not fit for Hardware (FoE Error Code 13 (0x800D) of slave)
-
EC_E_FOE_ERRCODE_NO_FILE
0x9811006F: SLV: ERROR FoE: No file to read (FoE Error Code 15 (0x800F) of slave)
-
EC_E_NO_FOE_SUPPORT_BS
0x9811010F: APP: ERROR FoE: Protocol not supported in boot strap (e.g. Application requested FoE in Bootstrap although slave does not support this)
-
EC_E_FOE_ERRCODE_MAX_FILE_SIZE
0x9811017A: APP: ERROR FoE: File is bigger than max file size (e.g. Slave returned more data than the buffer provided by application can store.)
-
EC_E_FOE_ERRCODE_FILE_HEAD_MISSING
0x98130001: SLV: ERROR FoE: File header does not exist (FoE Error Code 16 (0x8010) of slave)
8.7. Servo Drive Profil over EtherCAT (SoE) Error Codes
-
EC_E_SOE_ERRORCODE_MIN_UNDERSIZE
0x9811008A: ERROR SoE: Minimum input value undersize in transmission
-
EC_E_SOE_ERRORCODE_MAX_UNDERSIZE
0x9811008F: ERROR SoE: Maximum input value undersize in transmission
-
EC_E_SOE_ERRORCODE_DATA_MIN_LIMIT
0x98110098: ERROR SoE: Data item less than minimum input value limit
-
EC_E_SOE_ERRORCODE_DATA_MAX_LIMIT
0x98110099: ERROR SoE: Data item exceeds maximum input value limit
-
EC_E_SOE_ERRORCODE_TEMP_UNCHANGE
0x9811009C: ERROR SoE: Data item temporary unchangeable (in AT or MDT)
-
EC_E_SOE_ERRORCODE_TEMP_UNCHANGE1
0x9811009E: ERROR SoE: Data item temporary unchangeable (parameter or opmode)
-
EC_E_SOE_ERRORCODE_DRIVE_NO
0x98110103: ERROR SoE: Response drive number not identical with requested drive number
8.8. Remote API Error Codes
-
EC_E_SOCKET_DISCONNECTED
0x9811017D: RAS: Socket disconnected (e.g. IP connection terminated or lost)
-
EMRAS_E_MULSRVDISMULCON
0x98110183: RAS: Connect 2nd server denied because Multi Server support is disabled (obsolete)
-
EMRAS_E_LOGONCANCELLED
0x98110184: RAS: Logon canceled (Server-side connection reject while opening a client connection.)
-
EMRAS_E_INVALIDVERSION
0x98110186: RAS: Invalid Version (Connection reject because of using mismatching protocol versions on client and server side)
-
EMRAS_E_INVALIDACCESSCONFIG
0x98110187: RAS: Access configuration is invalid (e.g. SPoC access configuration invalid)
-
EMRAS_E_ACCESSLESS
0x98110188: RAS: No access to this call at this access level (e.g. a higher SPoC access level is needed to use the called Remote API function)
-
EMRAS_EVT_SERVERSTOPPED
0x98110191: RAS: Server stopped (e.g. connection dropped because of Remote API Server stop)