4.16. FreeRTOS
4.16.1. Setting up and running EcMasterDemo on Xilinx Zynq UltraScale+ (ZCU104) and Xilinx Zynq-7000 (ZC702 Evaluation Kit)
Install Xilinx SDK 2018.2 or Install Xilinx Vitis IDE 2022.2
4.16.1.1. How to create the demo applications for Xilinx Zynq
- Create ENI file for EtherCAT configuration.
xxd.exeis capable of converting ENI files to a C file as array, e.g.xxd.exe -i eni.xml ENI.cReplace ENI.c file with generated one.
- Create a BSP project
Based on the delivered hardware project, replace the settings file with the one from the package:
for Xilinx SDK
setws . importprojects . createbsp -name ZCU104_bsp_cortexa53 -hwproject ZCU104_hw_platform -proc psu_cortexa53_0 -arch 64 -os freertos10_xilinx createbsp -name ZCU104_bsp_cortexr5 -hwproject ZCU104_hw_platform -proc psu_cortexr5_0 -os freertos10_xilinx createbsp -name ZC702Rev_bsp -hwproject ZC702Rev_hw_platform -proc ps7_cortexa9_0 -os freertos10_xilinx createbsp -name ZedBoard_bsp -hwproject ZedBoard_hw_platform -proc ps7_cortexa9_0 -os freertos10_xilinx createbsp -name ZC701ZynqDimm_bsp -hwproject ZC701ZynqDimm_hw_platform -proc ps7_cortexa9_0 -os freertos10_xilinx
- replace:
../<BSP name>/<core name>/libsrc/freertos10_xilinx_v1_1/src/FreeRTOSConfig.h
for Vitis IDE
set PATH=C:\Xilinx\Vitis\2022.2\bin;%PATH% set BUILD_SEVENZIP="C:\Program Files\7-Zip\7z.exe" @echo "Build with Xilinx Software Commandline Tool (XSCT)" REM Create Xilinx BSP's @echo "Create Xilinx BSP's" pushd %BUILDOUTPUT%\Workspace\FreeRTOS_Zynq_Vitis\ call xsct.bat ZCU104\platform.tcl call xsct.bat ZCU106\platform.tcl call xsct.bat Kria_KR260\platform.tcl call xsct.bat zc702\platform.tcl
- replace:
../<BSP name>/psu_cortexr5_0/FreeRtos32BitR5/bsp/psu_cortexr5_0/libsrc/freertos10_xilinx_v1_12/src/FreeRTOSConfig.h
For the new BSP project, just use the same BSP name and core as in the package.
4.16.1.2. How to run the EC-Master demo applications on Xilinx Zynq
- Via USB debugger
Load the application with to the chosen core.
- Via SD card
By creating a
BOOT.binfile, e.g.:- for Xilinx SDK
bootgen -w on -image ../EcMasterDemo_ZCU104_cortexa53.bif -arch zynqmp -o BOOT.bin
Maybe adjust the boot setting switches on the board
4.16.2. Setting up and running EcMasterDemo on TI AM64x EVM for R5 Core
- Install MCU-PLUS-SDK-AM64X 08.01.00.36
Code Composer Studio 11.1 or newer
4.16.2.1. How to create the demo applications on TI AM64x
- Create ENI file for EtherCAT configuration.
xxd.exeis capable of converting ENI files to a C file as array, e.g.xxd.exe -i eni.xml ENI.cReplace ENI.c file with generated one.
- rebuild BSP for the correct performance measurement
Change: ti/mcu_plus_sdk_am64x_08_01_00_36/source/kernel/freertos/config/am64x/r5f/FreeRTOSConfig.h
#define configUSE_IDLE_HOOK (0)or:
ti/mcu_plus_sdk_am64x_08_01_00_36/source/kernel/freertos/portable/TI_ARM_CLANG/ARM_CR5F/port.c
vApplicationIdleHook()replace“wfi”with“nop”
4.16.2.2. How to run the EC-Master demo applications on TI AM64x
- Run via Debugger
Follow getting started guide to flash the UART loader into the internal memory. Load the application with and the Target Configuration to the R5F_0 core.
- Run via µSD card
Adjust and rebuild sbl_sd boot example in the mcu_plus_sdk. in main.c replace
#define BOOTLOADER_APPIMAGE_MAX_FILE_SIZE (0x60000) /* Size of section MSRAM_2 specified in linker.cmd */
uint8_t gAppImageBuf[BOOTLOADER_APPIMAGE_MAX_FILE_SIZE] __attribute__((aligned(128), section(".bss.filebuf")));
with
#define BOOTLOADER_APPIMAGE_MAX_FILE_SIZE (0x800000) /* This has to match the size of DDR section in linker.cmd */
uint8_t gAppImageBuf[BOOTLOADER_APPIMAGE_MAX_FILE_SIZE] __attribute__((aligned(128), section(".bss.filebuf")));
4.16.3. Setting up and running EcMasterDemo on TI J784s4 EVM for R5 Core
Support for TiEnetCpswg on J784s4 is currently limited to TI J784S4X EVM with FreeRTOS in polling mode. It’s working with ti-processor-sdk-rtos-j784s4-evm-08_06_01_03.
- Install PROCESSOR-SDK-RTOS-J784S4 Version: 08.06.01.03
Code Composer Studio 11.2 or newer
4.16.3.1. How to create the demo applications on TI J784s4
- Create ENI file for EtherCAT configuration.
See TI AM64x
- Adjust FreeRTOSConfig.h
See
…/ti-processor-sdk-rtos-j784s4-evm-08_06_01_03/pdk_j784s4_08_06_01_03/packages/ti/kernel/freertos/config/j784s4/r5f/FreeRTOSConfig.hTurn off
configUSE_IDLE_HOOK, else vApplicationIdleHook() is called withasm("WFI");is used. WithWFIthe ARM ccnt counter sleep and the performance measurement fails (WFIcould also be replaced byNOP).Heap size is not set with
configTOTAL_HEAP_SIZEit’s configured in the linker scriptlinker_r5_freertos.lds
4.16.3.2. How to run the EC-Master demo applications on TI J784s4
- Run via Debugger
See TI AM64x
- Run via µSD card
See sbl_mmcsd example